roadmap meta-imx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

roadmap meta-imx

4,036件の閲覧回数
Jeroen_H
Contributor III

Hi !

We are planning to upgrade our Yocto build environment.

Currently, the meta-imx layer is available for Zeus and Hardknott.

Are there any plans to update the BSP meta-imx to Honister and/or Kirkstone? 
Is there a roadmap for this somewhere with estimated release dates?

Thank you very much.

Jeroen.

ラベル(1)
タグ(2)
0 件の賞賛
返信
4 返答(返信)

3,532件の閲覧回数
fenil
Contributor I

Hi, is there a plan to upgrade the BSP to Kirkstone in near future ?
Since honister support will not be available post MAY-2022. 

0 件の賞賛
返信

4,015件の閲覧回数
Jeroen_H
Contributor III

Hi Igor, 

Thanks for answering!
Do you have contact details of the local marketing office in Europe so I can contact them ?


Kind regards,
Jeroen.

0 件の賞賛
返信

4,013件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

local NXP Sales Offices:


http://www.nxp.com/about/about-nxp/worldwide-locations:GLOBAL_SITES

 

Best regards
igor

0 件の賞賛
返信

4,019件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jeroen

 

yes there plans to update the BSP to Honister in next year, more detailed information

can be obtained from local marketing office.

 

Best regards
igor