resizing picture using IPU on IMX53

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

resizing picture using IPU on IMX53

跳至解决方案
2,986 次查看
markusturban
Contributor I

Hello Community,

I want to resize a picture (twice: 1/2 and 1/4) which is captured by a camera using the IPU. I'm working on a Linuxkernel (freescale) and I'm using the IPU-HL Libs. (mxc_ipu_hl_lib.h)

The IPU does not resize, its cropping my picture when I'm doing following:

- captured image is grayscale

- size 1280 x 1024

Whats wrong with my code? Thank's for help :smileyhappy:

1) "Main-function" - in constructor of "ImageDisplay" [startIPU] is called

void ImageDisplay::setImage(void* buffer, int CamPitch)

{

    cv::Mat m_lastImage;

    //size of picture is 1280 x 1024

    int x = 1280/2;

    int y = 1024/2;

    //copy captured picture to buffer

    memcpy(buf[1],buffer,test_handle.input.width * test_handle.input.height);

    updateIPU(&test_handle, x, y);

    //saving image using OpenCV

    m_lastImage = cv::Mat(y, x, CV_8UC1, buf[1], CamPitch);

    cv::imwrite("img05.bmp", m_lastImage );

    

    x/=2;

    y/=2;

    memcpy(buf[1],buffer,test_handle.input.width * test_handle.input.height);

    updateIPU(&test_handle, x, y);

    m_lastImage = cv::Mat(y, x, CV_8UC1, buf[1], CamPitch);

    cv::imwrite("img025.bmp", m_lastImage );

}

2. Initialisation of IPU

int ImageDisplay::startIPU(ipu_test_handle_t * test_handle)

{

    if ((fd_fb = open("/dev/fb0", O_RDWR, 0)) < 0)

    {

        printf("Unable to open /dev/fb0\n");

        ret = -1;

    }

    if ( ioctl(fd_fb, FBIOGET_VSCREENINFO, &fb_var) < 0)

    {

        printf("Get FB var info failed!\n");

        ret = -1;

    }

  

    if ( ioctl(fd_fb, FBIOGET_FSCREENINFO, &fb_fix) < 0)

    {

        printf("Get FB fix info failed!\n");

        ret = -1;

    }

    if(fb_var.yres_virtual != 3*fb_var.yres)

    {

        fb_var.yres_virtual = 3*fb_var.yres;

        if ( ioctl(fd_fb, FBIOPUT_VSCREENINFO, &fb_var) < 0)

        {

            printf("Get FB var info failed!\n");

            ret = -1;

        }

    }

    screen_size = fb_var.yres * fb_fix.line_length;

    fb[0] = mmap(NULL, 3 * screen_size, PROT_READ | PROT_WRITE, MAP_SHARED,

            fd_fb, 0);

    if (fb[0] == MAP_FAILED)

    {

        printf("fb buf0 mmap failed, errno %d!\n", errno);

        ret = -1;

    }

    fb[1] = (void *)((char *)fb[0]);

    fb[0] = (void *)((char *)fb[1] + screen_size);

    fb[2] = (void *)((char *)fb[1] + 2*screen_size);

    /* use I420 input format as fix*/

    test_handle->mode = OP_STREAM_MODE;

    test_handle->input.width = 1280;

    test_handle->input.height = 1024;

    test_handle->input.fmt = v4l2_fourcc('I', '4', '2', '0');

    if (fb_var.bits_per_pixel == 24)

        test_handle->output.fmt = v4l2_fourcc('B', 'G', 'R', '3');

    else

        test_handle->output.fmt = v4l2_fourcc('R', 'G', 'B', 'P');

    test_handle->output.width = fb_var.xres;

    test_handle->output.height = fb_var.yres;

    size = test_handle->input.width * test_handle->input.height * 3;

    ret = dma_memory_alloc(size, BUF_CNT, paddr, buf);

    if ( ret < 0) {

        printf("dma_memory_alloc failed\n");

    }

  

    test_handle->input.user_def_paddr[0] = paddr[0];

    test_handle->input.user_def_paddr[1] = paddr[1];

     //init buffer (writing values)

    gen_fill_pattern((char*)buf[0], test_handle->input.width, test_handle->input.height);

    gen_fill_pattern((char*)buf[1], test_handle->input.width, test_handle->input.height);

    ret = mxc_ipu_lib_task_init(&(test_handle->input), NULL, &(test_handle->output), test_handle->mode, test_handle->ipu_handle);

    if (ret < 0)

    {

        printf("mxc_ipu_lib_task_init failed!\n");

    }

    return 0;

}

3.) Finally calling the update function

int ImageDisplay::updateIPU(ipu_test_handle_t * test_handle, int x, int y)

{

    test_handle->output.width = x;

    test_handle->output.height = y;

    if(mxc_ipu_lib_task_buf_update(test_handle->ipu_handle, paddr[1], 0, 0, NULL, NULL) < 0)

        return -1;

    else

        return 0;

}




标签 (1)
0 项奖励
回复
1 解答
2,115 次查看
rogerio_silva
NXP Employee
NXP Employee

Hi Markus,

I don't know if it helps, but you can take a look on this rotation code:

https://github.com/rogeriorps/ipu-examples/blob/master/mx5/rotation/example1/rot_ex1.c

Take off the rotation part (or run with rotation=0) and change the output size to the desired image size changing the following lines:

test_handle.output.width = fb_var.xres;

test_handle.output.height = fb_var.yres;

Rgds

Rogerio

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,115 次查看
markusturban
Contributor I

Hello,

as I assumend its not working with gstreamer.

Can anybody provide a code-snippet for resizing pics with IPU and HL-Libs (mxc_ipu_hl_lib.c) ?

Thx,

Markus

0 项奖励
回复
2,116 次查看
rogerio_silva
NXP Employee
NXP Employee

Hi Markus,

I don't know if it helps, but you can take a look on this rotation code:

https://github.com/rogeriorps/ipu-examples/blob/master/mx5/rotation/example1/rot_ex1.c

Take off the rotation part (or run with rotation=0) and change the output size to the desired image size changing the following lines:

test_handle.output.width = fb_var.xres;

test_handle.output.height = fb_var.yres;

Rgds

Rogerio

0 项奖励
回复
2,115 次查看
BrilliantovKiri
Senior Contributor I

Hello, Markus!

I solve this with Gstreamer mfw_ipu_csc plugin, please see attache.

I hope this helps.

0 项奖励
回复
2,115 次查看
markusturban
Contributor I

Hello Kirill,

thanks for your reply.

I'm not using v4linux. So I'm not sure if gstreamer(+plugin) is working for me. My cam-driver (closed source) is running as a service and is providing a void* field in memory by an API. I want to copy this field in DMA and IPU should resize it. The Camera is connected by USB.

In the .patch-file a file/folder "src/video/ipu_csc/src/mfw_gst_ipu_csc.c" is mentioned. I can't find this file in my toolchain directory...

Can you tell me where I can find "src/mfw_gst_ipu_csc.c". Maybe you can also post a little code-example....

Many thanks,

Markus

0 项奖励
回复
2,115 次查看
BrilliantovKiri
Senior Contributor I

Hello, Markus!

You can find full source in gst-fsl-plugin-2.0.3/src/video/ipu_csc/src/mfw_gst_ipu_csc.c.