repo init error from git.freescale.com

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

repo init error from git.freescale.com

1,825 Views
zhangzy
Contributor I

I'm trying to pull the baseline code  from the git.freescale.

 I 've set the http_proxy and https_proxy, but connection error happened when repo init,how should I resolve it?

 $repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1.15-1.0.0_ga
Get https://gerrit.googlesource.com/git-repo/clone.bundle
Get https://gerrit.googlesource.com/git-repo
remote: Finding sources: 100% (66/66)
remote: Total 66 (delta 21), reused 66 (delta 21)
Unpacking objects: 100% (66/66), done.
From https://gerrit.googlesource.com/git-repo
   ffb4b89..a24671f  master     -> origin/master
Get git://git.freescale.com/imx/fsl-arm-yocto-bsp.git
fatal: unable to connect to git.freescale.com:
git.freescale.com: Name or service not known

0 Kudos
Reply
1 Reply

1,399 Views
joanxie
NXP TechSupport
NXP TechSupport

pls try to set none to poxy.

0 Kudos
Reply