regain debug access RT1176

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

regain debug access RT1176

864件の閲覧回数
ingdb
Contributor III

Hello all,

I have a custom board based on the RT1176 processor. Everything was working fine but when testing/debugging something around FlexSPI I loaded a program on the board that prevent the debugger to connect. I got always the same error message, when trying to debug the board but also when trying to erase the flash with the GUI tool

Probe Firmware: MCU-LINK Pro (r0CF) CMSIS-DAP V2.263 (NXP Semiconductors)
Serial Number:  EPQGLZRRF3CNH
VID:PID:  1FC9:0143
USB Path: \\?\hid#vid_1fc9&pid_0143&mi_00#c&35210a53&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
connection failed - Em(01). Cannot find MEM-AP selected by core index (check target power).. Retrying
Failed on connect: Em(01). Cannot find MEM-AP selected by core index (check target power)
Connected&Reset. Was: NotConnected. DpID: 6BA02477. CpuID: 00000000. Info: <None>

As I've seen on the RT1020 eval board it is possible to brick a board by software. On the RT1020 EVK the fix was easy (change bootmode and delete the flash) but how do I do this on my custom board? I don't have a dip switch for the boot modes and I don't want to desolder resistors. Is there any other way to recover such a board?

 

best regards

Matthias

ラベル(1)
0 件の賞賛
返信
0 返答(返信)