reboot fail

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

reboot fail

2,405 次查看
tsgenius
Contributor I

Hi,everyone

I have got a reboot problem with IMX6Q sabresd on my custmer board and described as following:

1.Linux BSP 4.1.0,when I enter reboot command,system will reboot fail in most cases,only about 10 percentage system reboot success.I have refer the following site:

        https://community.freescale.com/message/408776#408776

   And comment out "bic r0, r0, #0x0006",but it is not useful.

2.Accidental,I tried BSP rel_imx_3.0.35_12.09.01,and find that reboot command always runs successfully.I have compared the following function with the two BSP:

arm_machine_restart    cpu_proc_fin    arch_reset

There are some differences in arch_reset.Then I modify BSP 4.1.0 code arch_reset function same as rel_imx_3.0.35_12.09.01's,but reboot command also fails in most cases

Anyone can help me?

标签 (1)
0 项奖励
回复
2 回复数

1,838 次查看
tsgenius
Contributor I

PS:reset command in u-boot runs successfully every time

0 项奖励
回复

1,838 次查看
jimmychan
NXP TechSupport
NXP TechSupport

On sabresd board, it use WDOG2 output to reset external PMIC. If your board does not reboot properly, you can check your WDOG2 output pin config. For your information, please check the content of the patch "2270-ENGR00233366-4-WDOG-LDO_BYPASS-fix-wdog2-to-reset-ex.patch". You can find this patch in the linux/patches/ folder.

0 项奖励
回复