.realtime linux support with i.Mx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

.realtime linux support with i.Mx

1,989件の閲覧回数
zanzibar
Contributor I

Hi,

We need to design an application with realtime Linux (RTAI or Xenomai).

Which i.Mx families can we use ?

on which family has Xenomai or RTAI been ported ?

Thanks,

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,676件の閲覧回数
sinanakman
Senior Contributor III

Hi Maxime, not exactly what you are asking but Linux RT patches are running fine

on iMX6 (e.g. sabresd).

Hope this helps

Sinan Akman

0 件の賞賛
返信

1,676件の閲覧回数
Yuri
NXP Employee
NXP Employee

  IMX6 may be used for real time Linux, but Freescale does not support it, at least till now. 

Xenomai on i.MX6D


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信