.realtime linux support with i.Mx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

.realtime linux support with i.Mx

1,985 Views
zanzibar
Contributor I

Hi,

We need to design an application with realtime Linux (RTAI or Xenomai).

Which i.Mx families can we use ?

on which family has Xenomai or RTAI been ported ?

Thanks,

Labels (1)
0 Kudos
Reply
2 Replies

1,672 Views
sinanakman
Senior Contributor III

Hi Maxime, not exactly what you are asking but Linux RT patches are running fine

on iMX6 (e.g. sabresd).

Hope this helps

Sinan Akman

0 Kudos
Reply

1,672 Views
Yuri
NXP Employee
NXP Employee

  IMX6 may be used for real time Linux, but Freescale does not support it, at least till now. 

Xenomai on i.MX6D


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply