read fuses from Linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

read fuses from Linux

7,450 次查看
antonio_santagi
Contributor IV

Hello,

regarding iMX8MM, is it possible to read fuses status from Linux ?

I know about commands to read and program them from U-Boot, but I haven't found anything mentioned about Linux, in the Yocto BSP user guide , for example. So, I guess it's not possible, or is it ?

 

thank you

标签 (2)
0 项奖励
回复
4 回复数

6,400 次查看
KingleyMarve
Contributor I

I noticed that this thread is a couple of years old, but I hope my response can still be helpful. One tool you can try is ""imxotp,"" which is a Linux user space driver for reading fuses on i.MX SoCs. This tool can be used to read fuses from Linux by specifying the fuse bank and word you want to read. Another tool you can use is ""fuseread,"" which is a simple utility that allows you to read fuses by specifying the SoC and fuse bank. Also, if you need any support related to CentOS 7, feel free to check out this link https://tuxcare.com/extended-lifecycle-support/centos-7-extended-support/. It could come in handy for your project.

0 项奖励
回复

7,436 次查看
antonio_santagi
Contributor IV

thank you ,

this is interesting. I checked on my device where we run a 4.19.35 Kernel .

I can see this : 

# ls /sys/devices/platform/30350000.ocotp-ctrl/
driver driver_override modalias of_node power subsystem uevent

So I can't find that node 

/sys/devices/platform/30350000.ocotp-ctrl/imx-ocotp0/nvmem

they are referring to in the post you linked.

I checked also in the subfolders and I can't see any imx-ocotp0/nvmem.

 

0 项奖励
回复

7,416 次查看
joanxie
NXP TechSupport
NXP TechSupport

I checked the source code of 4.19.35, the dtsi file is the same as 4.14.98 about OCOTP, you should get this, try to build again

"https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/fsl-imx8mm.d...

ocotp: ocotp-ctrl@30350000 {
		compatible = "fsl,imx8mq-ocotp", "fsl,imx7d-ocotp", "syscon";
		reg = <0 0x30350000 0 0x10000>;
		clocks = <&clk IMX8MM_CLK_OCOTP_ROOT>;
		/* For nvmem subnodes */
		#address-cells = <1>;
		#size-cells = <1>;
	};

 

0 项奖励
回复

7,442 次查看
joanxie
NXP TechSupport
NXP TechSupport
0 项奖励
回复