read fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

read fail

1,805件の閲覧回数
jiema
Contributor I

Hi, Engineer

    when I type the command , dmesg to watch the kernel information , the information is the following :

FIFO_RD_AUX_LSB read fails
FIFO_RD_AUX_MSB read fails
FIFO_RD_AUX_LSB read fails
FIFO_RD_AUX_MSB read fails
FIFO_RD_AUX_LSB read fails
FIFO_RD_AUX_MSB read fails
FIFO_RD_AUX_LSB read fails
FIFO_RD_AUX_MSB read fails
FIFO_RD_AUX_LSB read fails
FIFO_RD_AUX_MSB read fails
FIFO_RD_AUX_LSB read fails

There are no other information to be listed, just the information above . My core board is imx6q . I need you help, thanks!

ラベル(3)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,685件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jie

seems this message is from ..drivers/input/touchscreen/max11801_ts.c

Is this chip used in custom board, in general one can debug it using
AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors
http://www.nxp.com/assets/documents/data/en/application-notes/AN4553.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,685件の閲覧回数
jiema
Contributor I

Hi, igorpadykov

    I am glad to see your repay,  The chip max11801 is used for touch panel controller in my custom board. The operation to touch panel is normal. I want to watch the kernel information using the command dmesg. but now It fails. The document will be useful when I debug. Now I just need to watch , not to debug. 

 Best regards

 Allen

0 件の賞賛
返信