rcu_preempt issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

rcu_preempt issue

4,933件の閲覧回数
57063778
Contributor II

Hi,all

 

    I am facing a Linux kernel dump issue after running about 48 hours. The BSP is Yocto with Linux 3.14.28 and the CPU is imx6Q. The dump information is as follow and how to fix the issue? Thanks in advance.

 

Dec 5 05:36:35 linux user.err kernel: INFO: rcu_preempt detected stalls on CPUs/tasks: { 2} (detected by 1, t=2102 jiffies, g=45107986, c=45107985, q=5227)
Dec 5 05:36:35 linux user.info kernel: Task dump for CPU 2:
Dec 5 05:36:35 linux user.info kernel: grep R running 0 1231 1228 0x00000002
Dec 5 05:36:35 linux user.warn kernel: [<80716800>] (__schedule) from [<a9c94020>] (0xa9c94020)

タグ(1)
6 返答(返信)

4,079件の閲覧回数
57063778
Contributor II

Hi igor,

   Thanks for your reply.

   Will the linux "https://source.codeaurora.org/external/imx/linux-imx -b imx_4.14.78_1.0.0_ga" fix the RCU issue? Or which version can fix the issue?

0 件の賞賛
返信

4,079件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

please try latest described on nxp official software page

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

Best regards
igor

4,079件の閲覧回数
57063778
Contributor II

Hi igorpadykov,

    The URL"https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser..." always redirect to "i.MX Software|NXP ". And I can not get the right information. Would you please send the according material to my email: xuyongxian@kehua.com.  Thank you very much.

0 件の賞賛
返信

4,079件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 57063778@qq.com 

actually it is the same link, you can find all relevant documentation on

i.MX Software|NXP 

Best regards
igor

4,079件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

4,079件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

usually rcu_preempt errors happen due to arm/gpu bugs which were fixed in later nxp

linux releases (they are documented in Release Notes found on below link)

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------