raw data processing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

raw data processing

3,696 Views
michael_irsfeld
Contributor I

Hello,

i'm searching for a SoC. For a project i would like to embedd two cameras that send raw data (Bayer12bit). The datasheet of i.MX6Q tells that the camera interface is possible to get generic data. But is it possible to process data into a MPEG video stream on i.MXQ?

Thanks!
Michael

0 Kudos
Reply
5 Replies

3,475 Views
joanxie
NXP TechSupport
NXP TechSupport

for 12-bit raw data, pls refer to the link as below:

https://community.nxp.com/thread/320618 

0 Kudos
Reply

3,475 Views
michael_irsfeld
Contributor I

Hello,

thanks for answer. But this link does not help.

My question is if it is possible to handle two 12-bit Bayer input (1080p30) and convert it to MPEG4-Stream.


Thanks.

Michael

0 Kudos
Reply

3,475 Views
joanxie
NXP TechSupport
NXP TechSupport

do you mean two bayer input conver to one mpeg-4 streaming?

0 Kudos
Reply

3,475 Views
michael_irsfeld
Contributor I

I'm new in image processing, so I don't know if i can convert it to two streams or into one. I want to see both camera pictures on my PC.

0 Kudos
Reply

3,475 Views
joanxie
NXP TechSupport
NXP TechSupport

if you need dual raw data, you can use MIPI + parallel camera, but let me reminder, imx6 IPU couldn't display directly, you can refer to the link I sent to you , then display them separately

0 Kudos
Reply