raw data processing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

raw data processing

3,724件の閲覧回数
michael_irsfeld
Contributor I

Hello,

i'm searching for a SoC. For a project i would like to embedd two cameras that send raw data (Bayer12bit). The datasheet of i.MX6Q tells that the camera interface is possible to get generic data. But is it possible to process data into a MPEG video stream on i.MXQ?

Thanks!
Michael

ラベル(5)
0 件の賞賛
返信
5 返答(返信)

3,503件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for 12-bit raw data, pls refer to the link as below:

https://community.nxp.com/thread/320618 

0 件の賞賛
返信

3,503件の閲覧回数
michael_irsfeld
Contributor I

Hello,

thanks for answer. But this link does not help.

My question is if it is possible to handle two 12-bit Bayer input (1080p30) and convert it to MPEG4-Stream.


Thanks.

Michael

0 件の賞賛
返信

3,503件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

do you mean two bayer input conver to one mpeg-4 streaming?

0 件の賞賛
返信

3,503件の閲覧回数
michael_irsfeld
Contributor I

I'm new in image processing, so I don't know if i can convert it to two streams or into one. I want to see both camera pictures on my PC.

0 件の賞賛
返信

3,503件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

if you need dual raw data, you can use MIPI + parallel camera, but let me reminder, imx6 IPU couldn't display directly, you can refer to the link I sent to you , then display them separately

0 件の賞賛
返信