r8169 hangup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

r8169 hangup

2,293 Views
kecan
Contributor I

linux kernel 3.14.28,board imx6q.

when start,hangup,log is:

pi_imx 2018000.ecspi: probed
vcan: Virtual CAN interface driver
CAN device driver interface
2090000.can supply xceiver not found, using dummy regulator
flexcan 2090000.can: device registered (reg_base=c0ae8000, irq=142)
2188000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
fec 2188000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00
fec 2188000.ethernet (unregistered net_device): Using random MAC address: e6:3d:a2:45:df:8c
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
r8169 Gigabit Ethernet driver 2.3LK-NAPI loaded
PCI: enabling device 0000:01:00.0 (0000 -> 0003)                          (hangup)

or

mac:a0bb3e61af7d
maskPrefixLen:24, 4294967040
A0:BB:3E:61:AF:7B,192.168.69.13,255.255.255.0,255.255.255.255
mac:a0bb3e61af7b
maskPrefixLen:24, 4294967040
Starting Dropbear SSH server: dropbear.
Starting rpcbind daemon...r8169 0000:01:00.0: Direct firmware load failed with error -2
r8169 0000:01:00.0: Falling back to user helper
r8169 0000:01:00.0 eth1: unable to load firmware patch rtl_nic/rtl8168g-2.fw (-2)
r8169 0000:01:00.0: MRRS = 512, MPS = 128
r8169 0000:01:00.0 eth1: link down
IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
done.
starting statd: done
Starting advanced power management daemon: No APM support in kernel
(failed.)
NFS daemon support not enabled in kernel
Starting syslogd/klogd: done
* Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon [ ok ]
Starting Telephony daemon
eth0 gw:192.168.69.1
A0:BB:3E:61:AF:7D,192.168.69.10,255.255.255.0,192.168.69.1
mac:a0bb3e61af7d
maskPrefixLen:24, 4294967040
A0:BB:3E:61:AF:7B,192.168.69.13,255.255.255.0,255.255.255.255
mac:a0bb3e61af7b
maskPrefixLen:24, 4294967040      (hangup)

Labels (1)
0 Kudos
Reply
1 Reply

2,159 Views
igorpadykov
NXP Employee
NXP Employee

Hi  zhenyang

problems with r8169 were reported often on web, one can try

miscellaneous suggestions, for example disbale r8168 or upgrade driver.

16.04 - r8168/r8169 RealTek driver module troubles - Ask Ubuntu 

R8169 intermittantly hangs on boot 

In general one can try to debug it using AN4553 Using Open Source Debugging Tools

for Linux on i.MX Processors
https://www.nxp.com/docs/en/application-note/AN4553.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply