"something wrong with firmware address settings" error in nand_bcb with uuu and U-Boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

"something wrong with firmware address settings" error in nand_bcb with uuu and U-Boot

跳至解决方案
2,964 次查看
JohnKlug
Senior Contributor I

My issue (after putting debug code in U-Boot) is that max_boot_stream_size is less than zero in nandbcb_set_boot_config() in U-Boot, which is found in arch/arm/mach-imx/cmd_nand_bcb.c.

I am using U-Boot 2020.04.

I see the following intermediate values (maxsize matches the size of the U-Boot partition of the NAND):

maxsize 0x100000
bootstream_1_address=0x200000
bootstream_2_address=0x180000

My U-Boot is of size 658432 or 0xA0C00.
Partition table:

device nand0 <gpmi-nand>, # parts = 7
 #: name                size            offset          mask_flags
 0: nandboot            0x00100000      0x00000000      0
 1: env1                0x00040000      0x00100000      0
 2: env2                0x00040000      0x00140000      0
 3: nandkernel          0x01000000      0x00180000      0
 4: nanddtb             0x00080000      0x01180000      0
 5: nandtee             0x00100000      0x01200000      0
 6: nandrootfs          0x1ed00000      0x01300000      0

Plenty of space for U-Boot.

Here are the nand parameters:

Device 0: nand0, sector size 256 KiB
  Page size       4096 b
  OOB size         256 b
  Erase size    262144 b
  subpagesize     4096 b
  options     0x40004200
  bbt options 0x00060000


So what is the cause?

0 项奖励
回复
1 解答
2,895 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Sorry for replying until today I was looking into code what will be the cause of this, if this still is useful for you, the minimum nandboot partition should be equal to both search areas plus two copies of the boot_stream_size.

This by following the formulas in the nandbcb_set_boot_config() and nandbcb_check_space() functions.

Will give that the following:
nandboot minimum size >= boot_cfg->search_area_size_in_bytes*2 + Boot_size*2

Where:

boot_cfg->search_area_size_in_bytes = g_boot_search_count * g_boot_search_stride
g_boot_search_count = 4  // definition
g_boot_search_stride = mtd->erasesize
boot_stream_size = file_size_of(bootstream);

i.e
boot_stream_size = 658432 (0xa0c00)
g_boot_search_stride = 262144 (0x40000)

Then:

boot_cfg->search_area_size_in_bytes = 4*262144 = 1048576 (0x100000)
nandboot >= 1048576*2 + 658432*2 = 3414016 (0x341800)

Hope this helps,
Best regards,
Aldo.

在原帖中查看解决方案

6 回复数
2,932 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you share the uboot log you see when 1MB uboot size is set and fails?

Also, please fin nandbcb documentation here:
https://source.codeaurora.org/external/imx/uboot-imx/commit/?h=imx_v2020.04_5.4.70_2.3.0&id=c548451f...

Best regards,
Aldo.

0 项奖励
回复
2,926 次查看
JohnKlug
Senior Contributor I

Thanks for pointing out the documentation.

Here is the end of the log, and the uuu.auto file.

U-Boot Output:

Device 0: nand0, sector size 256 KiB
  Page size       4096 b
  OOB size         256 b
  Erase size    262144 b
  subpagesize     4096 b
  options     0x40004200
  bbt options 0x00060000
baudrate=115200
bootargs=console=ttymxc0,115200 rdinit=/linuxrc clk_ignore_unused
bootcmd=nand read ${loadaddr} 0x180000 0x1000000;nand read ${fdt_addr} 0x1180000 0x80000;if test ${tee} = yes; then nand read ${tee_addr} 0x1200000 0x100000;bootm ${tee_addr} - ${fdt_addr};else bootz ${loadaddr} - ${fdt_addr};fi
bootcmd_mfg=run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else bootz ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;
bootdelay=5
console=ttymxc0
emmc_ack=1
emmc_dev=1
ethprime=eth1
fastboot_buffer=0x80800000
fastboot_bytes=a0c00
fdt_addr=0x83000000
fdt_high=0xffffffff
filesize=a0c00
initrd_addr=0x86800000
initrd_high=0xffffffff
kboot=bootz 
loadaddr=0x80800000
mfgtool_args=setenv bootargs console=${console},${baudrate} rdinit=/linuxrc clk_ignore_unused 
mtdparts=mtdparts=gpmi-nand:1m(nandboot),256k(env1),256k(env2),16m(nandkernel),512k(nanddtb),1m(nandtee),-(nandrootfs)
nand_erasesize=40000
nand_oobsize=100
nand_writesize=1000
sd_dev=1
serial#=201a79d2677f0fb5
splashimage=0x8c000000
tee=yes
tee_addr=0x84000000

Environment size: 1149/262139 bytes

device nand0 <gpmi-nand>, # parts = 7
 #: name		size		offset		mask_flags
 0: nandboot            0x00100000	0x00000000	0
 1: env1                0x00040000	0x00100000	0
 2: env2                0x00040000	0x00140000	0
 3: nandkernel          0x01000000	0x00180000	0
 4: nanddtb             0x00080000	0x01180000	0
 5: nandtee             0x00100000	0x01200000	0
 6: nandrootfs          0x1ed00000	0x01300000	0

active partition: nand0,0 - (nandboot) 0x00100000 @ 0x00000000

defaults:
mtdids  : nand0=gpmi-nand
mtdparts: 
device 0 offset 0x0, size 0xa0c00
something wrong with firmware address settings


uuu.auto script:

uuu_version 1.2.39

# @_flash.bin            | bootloader
# @_image   [_flash.bin] | image burn to nand, default is the same as bootloader

# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f u-boot.imx

FB: ucmd setenv fastboot_buffer ${loadaddr}
FB: download -f u-boot.imx
# Burn image to nandfit partition if needed
FB: ucmd if env exists nandfit_part; then nand erase.part nandfit; nand write ${fastboot_buffer} nandfit ${fastboot_bytes}; else true; fi;
FB: ucmd nand info
FB: ucmd printenv
FB: ucmd mtdparts
FB: ucmd erase.chip
FB: ucmd nandbcb init ${fastboot_buffer} nandboot ${fastboot_bytes}
FB: ucmd mtd list
FB: ucmd printenv fastboot_buffer
FB: download -f zImage

FB: ucmd nand write ${fastboot_buffer} nandkernel ${fastboot_bytes}
FB: download -f mtcap3.dtb
FB: ucmd nand write ${fastboot_buffer} nanddtb ${fastboot_bytes}
FB: download -f uTee-6ullevk
FB: ucmd nand write ${fastboot_buffer} nandtee ${fastboot_bytes}
FB: download -f core-image-minimal-test-imx6ull14x14evk.ubi
FB[-t 20000]: ucmd nand write ${fastboot_buffer} nandrootfs ${fastboot_bytes}
FB: Done

 

0 项奖励
回复
2,896 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Sorry for replying until today I was looking into code what will be the cause of this, if this still is useful for you, the minimum nandboot partition should be equal to both search areas plus two copies of the boot_stream_size.

This by following the formulas in the nandbcb_set_boot_config() and nandbcb_check_space() functions.

Will give that the following:
nandboot minimum size >= boot_cfg->search_area_size_in_bytes*2 + Boot_size*2

Where:

boot_cfg->search_area_size_in_bytes = g_boot_search_count * g_boot_search_stride
g_boot_search_count = 4  // definition
g_boot_search_stride = mtd->erasesize
boot_stream_size = file_size_of(bootstream);

i.e
boot_stream_size = 658432 (0xa0c00)
g_boot_search_stride = 262144 (0x40000)

Then:

boot_cfg->search_area_size_in_bytes = 4*262144 = 1048576 (0x100000)
nandboot >= 1048576*2 + 658432*2 = 3414016 (0x341800)

Hope this helps,
Best regards,
Aldo.

2,888 次查看
JohnKlug
Senior Contributor I

In this case, 4MiB seems reasonable for nandboot, which needs to be 2MiB+2*(U-Boot Size).

These parameters are decided by the CPU from what I understand?  And they are known to be adequate for all NANDs? The redundancy is adequate to allow for bad blocks and ECC requirements?

0 项奖励
回复
2,956 次查看
JohnKlug
Senior Contributor I

I increased the size of the u-boot partition to 4MB, and now nandbcb appears to work.  Is this optimal?  u-boot is 658432, as I said.

0 项奖励
回复
2,959 次查看
JohnKlug
Senior Contributor I

One more question.  Is there documentation for nandbcb?

0 项奖励
回复