"imxv4l2sink" is not showing/rendering prerolled frame.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"imxv4l2sink" is not showing/rendering prerolled frame.

10,802 Views
shiva_mudugal
Contributor I

Hi All,

I am using "imxv4l2sink" and I see that its not showing prerolled frame. It only played framed decoded after going into playing state. Can you please help to fix this ?

Labels (4)
0 Kudos
Reply
10 Replies

10,630 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shiva

please check tutorial on

https://developer.ridgerun.com/wiki/index.php/IMX6_GStreamer_Pipelines_-_SDK_Turrialba 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

10,630 Views
shiva_mudugal
Contributor I

Hi igorpadykov,

Thank for the response, but there is no mention of "imxv4l2sink" in the link. I think, implementation is lacking this feature. Can you please help.

-Regards,

Shiva Kumar

0 Kudos
Reply

10,622 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shive

please look at attached Release Notes (imxv4l2sink as Video render plugin) and its usage in Linux Guide.

Linux Binary Demo Files - i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo, i.MX 6SoloX

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_MX6QDLSOLOX&appType=license&location=null&... 

Best regards
igor

0 Kudos
Reply

10,622 Views
shiva_mudugal
Contributor I

Hi igor, 

Attachment is having only pre-built images of kernel and boot loader. It doesn't contain release notes you have mentioned. 

-Regards,

Shiva

0 Kudos
Reply

10,622 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shiva

attached red right is "Release Notes" document.

pastedImage_1.jpg

Best regards
igor

0 Kudos
Reply

10,622 Views
shiva_mudugal
Contributor I

HI igor, 

Any update on this ? 

-Regards,

Shiva

0 Kudos
Reply

10,622 Views
shiva_mudugal
Contributor I

Hi igor,

Please help with this issue. It looks like preroll frame rendering mechanism is missing in "imxv4l2sink". If so what can be done here ?

-Regards

Shiva

0 Kudos
Reply

10,622 Views
shiva_mudugal
Contributor I

Hi igor,

The issue can also be reproduced in another manner. If we use "imxv4l2sink" and pause the video, in PAUSE state if we seek, frame will not be updated. But if we play, playback will start from the seeked position.

-Regards,

Shiva

0 Kudos
Reply

10,622 Views
shiva_mudugal
Contributor I

Hi igor,

I was able to download the user guide from the below link. There is nothing which addresses this issue. We are using the same way its mentioned there.

https://community.nxp.com/docs/DOC-340120 

-Regards,

Shiva

0 Kudos
Reply

10,622 Views
shiva_mudugal
Contributor I

Hi igor, 

Attachments are missing. I don't see attached documents. Please send them again.

-Regards,

Shiva

0 Kudos
Reply