"boot kernel with command debug_uart2"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"boot kernel with command debug_uart2"

1,955 Views
xlin
Contributor III

Hi,

On the page 12 of AN4580(which is attached herewith),  there are some steps to put  the Sololite into system idle mode under the section 5.2.4.

What does  "boot kernel with command debug_uart2" mean?

Best Regards,

Xinsi Lin

Labels (3)
0 Kudos
Reply
1 Reply

1,863 Views
gusarambula
NXP TechSupport
NXP TechSupport

The wording seems confusing but it’s most likely referring to setting up the serial console to run the steps that follow on the document. This is similar to the setup from the other i.MX6 Power Measurement App Notes.

0 Kudos
Reply