"No device connected" using MFG Tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

"No device connected" using MFG Tool

2,026 次查看
lhchang
Contributor I

Hi Sir,

I use Windows 10. Device manager can recognize the board which means the configuration should be no problem. But, when I use mfg tool, it show "no device connected". Can you help me how to check this problem?

best regards,

Langston

标签 (1)
0 项奖励
回复
2 回复数

1,601 次查看
shivanipatel
Senior Contributor II

Hi, lh chang‌,


MFGTool detects the device in serial download mode only. The board should be in serial download mode.

Follow below instructions to enter into serial download mode :

  • Set Boot Mode DIP switch in Serial Download Mode for your board (if there is a dedicated BOOT Mode switch on board)
  • If the boot device is SD Card then do not inset SD Card into the slot while launching MFGTool vbs script. After the message "HID Compliant device" is displayed, the board enters into serial download mode. Then insert SD Card into the slot and start MFGTool to flash images.

Regards,

Shivani

0 项奖励
回复

1,601 次查看
joanxie
NXP TechSupport
NXP TechSupport

pls check if your mfgtool version is correct or not, then change another PC to test again, I can use mfgtool on my pc with windows 10

0 项奖励
回复