question for /dev/fb0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

question for /dev/fb0

2,332 Views
guojunqiang
Contributor II

Dears,

Could you please tell that whether the func cfb_imageblit(...) in file cfbimgblt.c used for ?

I am porting lcdc on IMX7D,I just want to know if function  cfb_imageblit is needed when open /dev/fb0 to flush image in userspace test code.

Thank you.

Labels (1)
0 Kudos
Reply
1 Reply

2,238 Views
igorpadykov
NXP Employee
NXP Employee

Hi keil

what bsp used in the case and driver source. Just

for reference one can look at driver descriptions in attached Linux Manual

sect.6.3.4 ELCDIF Frame Buffer, sect.6.4.5 Electrophoretic Display Controller (EPDC) Interface

Linux L4.14.78_1.0.0    link
https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.78_1.0.0_ga


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply