query for G2D

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

query for G2D

1,604件の閲覧回数
guojunqiang
Contributor II

Dear Sir,

I got below info from graphics user's guide.

1:Could you show below G2D source code?

pastedImage_1.png

2:where can I find G2D HAL code ?

3:I found libg2d.so from path:root/vendor/nxp/fsl-proprietary/fsl-dpu/lib/libg2.so.

what is it used for ? can you show me source code ?

4:from i.mx8,g2d is replaced by dpu,right ?

5:where can I find the dpu kernel & hal code base ?

6:which android & kernel version support dpu ? please show the source code link.

Thank you.

0 件の賞賛
返信
1 返信

1,517件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keil

for sources one can refer to  Chapter 5 Graphics Linux Manual

and sect.5.1.5 Source Code Structure included in Linux 4.19.35_1.1.0 Documentation

As described in sect.5.1.1 Introduction :

"The GPU driver kernel module source is in the kernel source tree, but the libraries are
delivered as binary only."

Please also check i.MX_Graphics_User's_Guide.pdf,

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信