qtpdf throws continously compile time errors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

qtpdf throws continously compile time errors

4,600件の閲覧回数
srinivas_123
Contributor III

I am using the i.MX8M Plus LPDDR4 EVK. I built the i.MX, Linux LF6.6.23_2.0.0 BSP version of Yocto.

I built the imx-image-full and, after that, I needed the SDK for imx-image-full. So, I used the command bitbake imx-image-full -c populate_sdk.

However, when I ran the populate_sdk command, it threw the following error:


-- Could NOT find Gn: Found unsuitable version "2118 (811d332bd905)", but the required version is exact "6.7.0" (found /home/deevia-pc001/camera_porting/imx-yocto-bsp/build/tmp/work/armv8a-poky-linux/qtpdf/6.7.0/recipe-sysroot-native/usr/bin/gn)

nxp forum link :link:https://community.nxp.com/t5/i-MX-Processors/Encounter-error-when-bitbake-qtwebengine-cconfigure-in-...

In one of the forums on NXP, they suggested adding the following line to local.conf:

BBMASK += "/meta-browser/meta-chromium/recipes-browser/chromium/gn-native_.*\.bb"

I added that line to the local.conf file. However, when I ran populate_sdk again, it threw a qtpdf compile error. I have attached logs of  errors. Can anyone help me resolve this issue?

thanks&Regards

srinivas

0 件の賞賛
返信
1 返信

4,550件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Try to comment out the meta-chromium layer in the bblayers.conf

Regards

Harvey

0 件の賞賛
返信