qtpaths is missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

qtpaths is missing

3,582件の閲覧回数
emollergren
Contributor II

I have built the `img-image-full` image on imx8mp evk, and would like to install PySide6 on it.

This guide is telling me that the Qt installation path should be used:

emollergren_0-1657267192688.png

 

Unfortunately, I couldn't find the `qtpaths` in my system:

emollergren_1-1657267244738.png

 

Where is the qtpaths installed?

 

 

 

タグ(1)
0 件の賞賛
返信
2 返答(返信)

3,573件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello emollegren,

 

Not sure about Qtpath since the path for QT is in the begginer of yocto with path, but this should be the path for installation: 5.15-0.0.1/sysroots/x86_64-pokysdk-linux/usr/bin/qt6/

Regards

0 件の賞賛
返信

3,568件の閲覧回数
emollergren
Contributor II

Hi, there.

Thanks for your quick reply.

The problem is that the PySide6 installer needs `qtpaths` execution to resolve the paths of qt binaries.

How can we add the `qtpaths`?

0 件の賞賛
返信