qtlocation and qtsystems fetch failed in Yocto Project 5.10.52_2.1.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

qtlocation and qtsystems fetch failed in Yocto Project 5.10.52_2.1.0

1,234 Views
wang12zhe
Contributor III

From 7ulp imx-yocto-L5.10.52_2.1.0 build - NXP Community,got the qt original repository has been removed,so update the local.conf refer 0001-fix-missing-qt-repository.patch,

Then start build image,but got below Error:

WARNING: qtlocation-5.15.2+gitAUTOINC+02a21217a9_d3101bbc22-r0 do_fetch: Failed to fetch URL git://gitlab.com/qtmirror/qtlocation-mapboxgl.git;name=qtlocation-mapboxgl;branch=upstream/qt-staging;protocol=https;destsuffix=git/src/3rdparty/mapbox-gl-native, attempting MIRRORS if available
WARNING: qtsystems-5.15.2+gitAUTOINC+e3332ee38d-r0 do_fetch: Failed to fetch URL git://gitlab.com/qtmirror/qtsystems.git;name=qtsystems;branch=dev;protocol=https, attempting MIRRORS if available
ERROR: qtsystems-5.15.2+gitAUTOINC+e3332ee38d-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; unset _PYTHON_SYSCONFIGDATA_NAME; export PATH="/opt/yocto-workspace/build/tmp/work/aarch64-poky-linux/qtsystems/5.15.2+gitAUTOINC+e3332ee38d-r0/recipe-sysroot-native/usr/bin:/opt/yocto-workspace/sources/poky/scripts:/opt/yocto-workspace/build/tmp/work/aarch64-poky-linux/qtsystems/5.15.2+gitAUTOINC+e3332ee38d-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/opt/yocto-workspace/build/tmp/work/aarch64-poky-linux/qtsystems/5.15.2+gitAUTOINC+e3332ee38d-r0/recipe-sysroot/usr/bin/crossscripts:/opt/yocto-workspace/build/tmp/work/aarch64-poky-linux/qtsystems/5.15.2+gitAUTOINC+e3332ee38d-r0/recipe-sysroot-native/usr/sbin:/opt/yocto-workspace/build/tmp/work/aarch64-poky-linux/qtsystems/5.15.2+gitAUTOINC+e3332ee38d-r0/recipe-sysroot-native/usr/bin:/opt/yocto-workspace/build/tmp/work/aarch64-poky-linux/qtsystems/5.15.2+gitAUTOINC+e3332ee38d-r0/recipe-sysroot-native/sbin:/opt/yocto-workspace/build/tmp/work/aarch64-poky-linux/qtsystems/5.15.2+gitAUTOINC+e3332ee38d-r0/recipe-sysroot-native/bin:/opt/yocto-workspace/sources/poky/bitbake/bin:/opt/yocto-workspace/build/tmp/hosttools"; export HOME="/home/aen"; LANG=C git -c core.fsyncobjectfiles=0 clone --bare --mirror https://gitlab.com/qtmirror/qtsystems.git /opt/yocto-download/git2/gitlab.com.qtmirror.qtsystems.git --progress failed with exit code 128, output:
Cloning into bare repository '/opt/yocto-download/git2/gitlab.com.qtmirror.qtsystems.git'...
fatal: could not read Username for 'https://gitlab.com': No such device or address

ERROR: qtsystems-5.15.2+gitAUTOINC+e3332ee38d-r0 do_fetch: Fetcher failure for URL: 'git://gitlab.com/qtmirror/qtsystems.git;name=qtsystems;branch=dev;protocol=https'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /opt/yocto-workspace/build/tmp/work/aarch64-poky-linux/qtsystems/5.15.2+gitAUTOINC+e3332ee38d-r0/temp/log.do_fetch.25873
ERROR: Task (/opt/yocto-workspace/sources/meta-qt5/recipes-qt/qt5/qtsystems_git.bb:do_fetch) failed with exit code '1'
ERROR: qtlocation-5.15.2+gitAUTOINC+02a21217a9_d3101bbc22-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; unset _PYTHON_SYSCONFIGDATA_NAME; export PATH="/opt/yocto-workspace/build/tmp/work/aarch64-poky-linux/qtlocation/5.15.2+gitAUTOINC+02a21217a9_d3101bbc22-r0/recipe-sysroot-native/usr/bin:/opt/yocto-workspace/sources/poky/scripts:/opt/yocto-workspace/build/tmp/work/aarch64-poky-linux/qtlocation/5.15.2+gitAUTOINC+02a21217a9_d3101bbc22-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/opt/yocto-workspace/build/tmp/work/aarch64-poky-linux/qtlocation/5.15.2+gitAUTOINC+02a21217a9_d3101bbc22-r0/recipe-sysroot/usr/bin/crossscripts:/opt/yocto-workspace/build/tmp/work/aarch64-poky-linux/qtlocation/5.15.2+gitAUTOINC+02a21217a9_d3101bbc22-r0/recipe-sysroot-native/usr/sbin:/opt/yocto-workspace/build/tmp/work/aarch64-poky-linux/qtlocation/5.15.2+gitAUTOINC+02a21217a9_d3101bbc22-r0/recipe-sysroot-native/usr/bin:/opt/yocto-workspace/build/tmp/work/aarch64-poky-linux/qtlocation/5.15.2+gitAUTOINC+02a21217a9_d3101bbc22-r0/recipe-sysroot-native/sbin:/opt/yocto-workspace/build/tmp/work/aarch64-poky-linux/qtlocation/5.15.2+gitAUTOINC+02a21217a9_d3101bbc22-r0/recipe-sysroot-native/bin:/opt/yocto-workspace/sources/poky/bitbake/bin:/opt/yocto-workspace/build/tmp/hosttools"; export HOME="/home/aen"; LANG=C git -c core.fsyncobjectfiles=0 clone --bare --mirror https://gitlab.com/qtmirror/qtlocation-mapboxgl.git /opt/yocto-download/git2/gitlab.com.qtmirror.qtlocation-mapboxgl.git --progress failed with exit code 128, output:
Cloning into bare repository '/opt/yocto-download/git2/gitlab.com.qtmirror.qtlocation-mapboxgl.git'...
fatal: could not read Username for 'https://gitlab.com': No such device or address

ERROR: qtlocation-5.15.2+gitAUTOINC+02a21217a9_d3101bbc22-r0 do_fetch: Fetcher failure for URL: 'git://gitlab.com/qtmirror/qtlocation-mapboxgl.git;name=qtlocation-mapboxgl;branch=upstream/qt-staging;protocol=https;destsuffix=git/src/3rdparty/mapbox-gl-native'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /opt/yocto-workspace/build/tmp/work/aarch64-poky-linux/qtlocation/5.15.2+gitAUTOINC+02a21217a9_d3101bbc22-r0/temp/log.do_fetch.25874
ERROR: Task (/opt/yocto-workspace/sources/meta-qt5/recipes-qt/qt5/qtlocation_git.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 5433 tasks of which 5431 didn't need to be rerun and 2 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 2 seconds

what's the root cause and how to do it?

 

 

0 Kudos
Reply
1 Reply

1,224 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You should try the latest BSP 5.15.72, but this fetch issue is due a bad server or you have problem with your proxy, let's wait some time if the server is down it will be up in couple of minutes

 

regards

 

0 Kudos
Reply