qt5 not running if kernel build outside of the yocto project with version changes

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

qt5 not running if kernel build outside of the yocto project with version changes

1,010 次查看
narasimhuluorug
Contributor III

Hello,

Any one can suggest where I am missing as below mentioned log. Here I am working with 3.14 kernel and building separately but in qt5 yocto project of fsl is some another kernel version. Please suggest any inputs.

:~# qt5demo-starter

QEglFSImx6Hooks will set environment variable FB_MULTI_BUFFER=2 to enable double buffering and vsync.

If this is not desired, you can override this via: export QT_EGLFS_IMX6_NO_FB_MULTI_BUFFER=1

[     1] HAL user version 5.0.11 build 19959 Aug  6 2014 03:02:58

[     2] HAL kernel version 5.0.11 build 25762

Segmentation fault

Best Regards,

Narasimha

0 项奖励
回复
1 回复

794 次查看
jimmychan
NXP TechSupport
NXP TechSupport

could you tell me why not build all the things together in yocto?

0 项奖励
回复