qemu support for imx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

qemu support for imx

5,131 Views
santhosha
Contributor II

Is there any way to test the imx bsp in qemu virtual environment?

Labels (1)
3 Replies

3,187 Views
josephzhou1
Contributor V

yes there are not have qemuimx8 machine ,

 

but if you only want to test minimal build you still can try it build poky machine as qemux86-64 , and run it by using  runqemu . thanks all.

Best Regards,
Joseph Zhou Jianhui / Senior Embedded Software Engineer, Singapore
0 Kudos
Reply

3,784 Views
Yuri
NXP Employee
NXP Employee

Hello,

   You may look at the following

IMX7 Hypervisor mode

Regards,

Yuri.

0 Kudos
Reply

3,784 Views
igorpadykov
NXP Employee
NXP Employee

Hi santosha

unfortunately qemu is not supported for i.MX platforms.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply