pulseaudio bluetooth

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
22,789件の閲覧回数
sergio_dorazio
Contributor IV

Hi, I am working with IMX6ULL EVK.

Now I want start pulseaudio on bluetooth, I follow the examples in BlueZ5 and A2DP Sink on Freescale i.MX6Q/DL SabreSD  or in Add tutorial: setting-up Bluetooth - PulseAudio by BertLindeman · Pull Request #24 · ev3dev/ev3dev.g... but I have problems.

Have you examples or a sequence of linux command to start pulseaudio on bluetooth in IMX6ULL EVK board ?

Regards,

Sergio D'Orazio.

0 件の賞賛
返信
1 解決策
21,681件の閲覧回数
sergio_dorazio
Contributor IV

Hi Diego,

The problem is the mtu dimension of my BT chip, it is 180 bytes.

I have solved the problem putting in /etc/pulse/default.pa this line

load-module module-bluetooth-discover autodetect_mtu=yes

and modifing the file backend-ofono.c , in the pulseaudio yocto module , the fixed mtu from 48 to 180.

(in this file there isn't autodetect_mtu manage and than I have fixed value set).

By.

Sergio.

元の投稿で解決策を見る

21 返答(返信)
21,524件の閲覧回数
sergio_dorazio
Contributor IV

Hello Diego,

my hardware bluetooth is cc2564 texas, but ,for example, the l2ping command work well and than I think my hardware module work.

This is my first experience with bluetooth and than I think that I need the correct sequence for software module configuration. I send you my module software version : Bluez v5.49 ,,, pulseaudio v11.1

I think I need the start correct sequence for this 2 modules.

Regard.

Sergio.

0 件の賞賛
返信
21,524件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Are you able to see the devices that you are willing to connect with bluetoothctl scan on? If yes, are you able to connect to that device?

Best regards,

Diego.

0 件の賞賛
返信
21,524件の閲覧回数
sergio_dorazio
Contributor IV

Hi Diego,

now I am working with my imx6ull and I want to send and receive audio from smartphone bluetooth or PC bluetooth or speaker bluetooth.

The actual situation is :

  1. - when I work with smartphone bluetooth scan is ok , the connection is ok, I can play audio from smartphone and I can record the file on imx6 and the file is correct. I cannot play audio on imx6 because there isn't "sink bluetooth card" in pulseaudio.
  2. when I work with PC bluetooth scan is ok but the connection is failed.
  3. when I work with speaker bluetooth scan is ok, the connection is ok, I can play audio from speaker and I can record the file on imx6 but the file is empty. I can play audio on imx6 and I can listen well on speaker.

I need that the 3 configuration work well but for the moment I need work with smatphone.

I send you some trace.

I am seeing very strange service active on smartphone (sdptool browse <MAC SMARTPHONE>):

root@imx6ull14x14evk:~# sdptool browse BC:A5:8B:A3:8C:3A
Browsing BC:A5:8B:A3:8C:3A ...
Service RecHandle: 0x10000
Service Class ID List:
  "Generic Attribute" (0x1801)
Protocol Descriptor List:
  "L2CAP" (0x0100)
    PSM: 31
  "ATT" (0x0007)
    uint16: 0x0001
    uint16: 0x0003

Service RecHandle: 0x10001
Service Class ID List:
  "Generic Access" (0x1800)
Protocol Descriptor List:
  "L2CAP" (0x0100)
    PSM: 31
  "ATT" (0x0007)
    uint16: 0x0014
    uint16: 0x001a

Service Name: Headset Gateway
Service RecHandle: 0x10003
Service Class ID List:
  "Headset Audio Gateway" (0x1112)
  "Generic Audio" (0x1203)
Protocol Descriptor List:
  "L2CAP" (0x0100)
  "RFCOMM" (0x0003)
    Channel: 2
Profile Descriptor List:
  "Headset" (0x1108)
    Version: 0x0102

Service Name: Handsfree Gateway
Service RecHandle: 0x10004
Service Class ID List:
  "Handsfree Audio Gateway" (0x111f)
  "Generic Audio" (0x1203)
Protocol Descriptor List:
  "L2CAP" (0x0100)
  "RFCOMM" (0x0003)
    Channel: 3
Profile Descriptor List:
  "Handsfree" (0x111e)
    Version: 0x0107

Service Name: AV Remote Control Target
Service RecHandle: 0x10005
Service Class ID List:
  "AV Remote Target" (0x110c)
Protocol Descriptor List:
  "L2CAP" (0x0100)
    PSM: 23
  "AVCTP" (0x0017)
    uint16: 0x0104
Profile Descriptor List:
  "AV Remote" (0x110e)
    Version: 0x0104

Service Name: Advanced Audio Source
Service RecHandle: 0x10006
Service Class ID List:
  "Audio Source" (0x110a)
Protocol Descriptor List:
  "L2CAP" (0x0100)
    PSM: 25
  "AVDTP" (0x0019)
    uint16: 0x0103
Profile Descriptor List:
  "Advanced Audio" (0x110d)
    Version: 0x0103

Service RecHandle: 0x10007
Service Class ID List:
  "AV Remote" (0x110e)
  "AV Remote Controller" (0x110f)
Protocol Descriptor List:
  "L2CAP" (0x0100)
    PSM: 23
  "AVCTP" (0x0017)
    uint16: 0x0104
Profile Descriptor List:
  "AV Remote" (0x110e)
    Version: 0x0104

Service Name: Android Network Access Point
Service Description: NAP
Service RecHandle: 0x10008
Service Class ID List:
  "Network Access Point" (0x1116)
Protocol Descriptor List:
  "L2CAP" (0x0100)
    PSM: 15
  "BNEP" (0x000f)
    Version: 0x0100
    SEQ8: 0 6
Language Base Attr List:
  code_ISO639: 0x656e
  encoding:    0x6a
  base_offset: 0x100
Profile Descriptor List:
  "Network Access Point" (0x1116)
    Version: 0x0100

Service Name: Android Network User
Service Description: PANU
Service RecHandle: 0x10009
Service Class ID List:
  "PAN User" (0x1115)
Protocol Descriptor List:
  "L2CAP" (0x0100)
    PSM: 15
  "BNEP" (0x000f)
    Version: 0x0100
    SEQ8: 0 6
Language Base Attr List:
  code_ISO639: 0x656e
  encoding:    0x6a
  base_offset: 0x100
Profile Descriptor List:
  "PAN User" (0x1115)
    Version: 0x0100

Service Name: OBEX Phonebook Access Server
Service RecHandle: 0x1000a
Service Class ID List:
  "Phonebook Access - PSE" (0x112f)
Protocol Descriptor List:
  "L2CAP" (0x0100)
  "RFCOMM" (0x0003)
    Channel: 19
  "OBEX" (0x0008)
Profile Descriptor List:
  "Phonebook Access" (0x1130)
    Version: 0x0102

Browsing BC:A5:8B:A3:8C:3A ...
Service Search failed: Invalid argument
Service Name: SMS/MMS
Service RecHandle: 0x1000b
Service Class ID List:
  "Message Access - MAS" (0x1132)
Protocol Descriptor List:
  "L2CAP" (0x0100)
  "RFCOMM" (0x0003)
    Channel: 4
  "OBEX" (0x0008)
Profile Descriptor List:
  "Message Access" (0x1134)
    Version: 0x0102

Browsing BC:A5:8B:A3:8C:3A ...
Service Search failed: Invalid argument
Service Name: OBEX Object Push
Service RecHandle: 0x1000c
Service Class ID List:
  "OBEX Object Push" (0x1105)
Protocol Descriptor List:
  "L2CAP" (0x0100)
  "RFCOMM" (0x0003)
    Channel: 5
  "OBEX" (0x0008)
Profile Descriptor List:
  "OBEX Object Push" (0x1105)
    Version: 0x0102

Browsing BC:A5:8B:A3:8C:3A ...
Service Search failed: Invalid argument
root@imx6ull14x14evk:~#

And you can see also "Service Search failed: Invalid argument", what means ?

IMX6 active service are :

root@imx6ull14x14evk:~# sdptool browse local
Browsing FF:FF:FF:00:00:00 ...
Service RecHandle: 0x10000
Service Class ID List:
  "PnP Information" (0x1200)
Profile Descriptor List:
  "PnP Information" (0x1200)
    Version: 0x0103

Browsing FF:FF:FF:00:00:00 ...
Service Search failed: Invalid argument
Service Name: Handsfree
Service RecHandle: 0x10001
Service Class ID List:
  "Handsfree" (0x111e)
  "Generic Audio" (0x1203)
Protocol Descriptor List:
  "L2CAP" (0x0100)
  "RFCOMM" (0x0003)
    Channel: 6
Profile Descriptor List:
  "Handsfree" (0x111e)
    Version: 0x0101

Service Name: Audio Source
Service RecHandle: 0x10002
Service Class ID List:
  "Audio Source" (0x110a)
Protocol Descriptor List:
  "L2CAP" (0x0100)
    PSM: 25
  "AVDTP" (0x0019)
    uint16: 0x0103
Profile Descriptor List:
  "Advanced Audio" (0x110d)
    Version: 0x0103

Service Name: Audio Sink
Service RecHandle: 0x10003
Service Class ID List:
  "Audio Sink" (0x110b)
Protocol Descriptor List:
  "L2CAP" (0x0100)
    PSM: 25
  "AVDTP" (0x0019)
    uint16: 0x0103
Profile Descriptor List:
  "Advanced Audio" (0x110d)
    Version: 0x0103

Service Name: Headset Voice gateway
Service RecHandle: 0x10004
Service Class ID List:
  "Headset Audio Gateway" (0x1112)
  "Generic Audio" (0x1203)
Protocol Descriptor List:
  "L2CAP" (0x0100)
  "RFCOMM" (0x0003)
    Channel: 12
Profile Descriptor List:
  "Headset" (0x1108)
    Version: 0x0102

root@imx6ull14x14evk:~#

With this new information have you an idea for resolve my problems ?

Regards.

Sergio.

0 件の賞賛
返信
21,524件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Can you please verify if you have your card name with

pactl list cards

Furthermore, verify that the active profile is a2dp_sink. Otherwise, it will not reproduce any sound. 

You should see something as below:

 

Card #3
Name: bluez_card.xx_xx_xx_xx_xx_xx #The xx is the MAC address of your Bluetooth device
Driver: module-bluez5-device.c
Owner Module: 23
Properties:
        device.description = "xx" #Here you will find the name of your device.
        device.string = "xx:xx:xx:xx:xx:xx" #This is also the MAC address of your Bluetooth device
        device.api = "bluez"
        device.class = "sound"
        device.bus = "bluetooth"
        device.form_factor = "headset"
        bluez.path = "/org/bluez/hci0/dev_xx_xx_xx_xx_xx_xx" #This is also the MAC address of your Bluetooth device
        bluez.class = "0x240404"
        bluez.alias = "xx"
        device.icon_name = "audio-headset-bluetooth"
        device.intended_roles = "phone"
Profiles:
        headset_head_unit: Headset Head Unit (HSP/HFP) (sinks: 1, sources: 1, priority: 20, available: yes)
        a2dp_sink: High Fidelity Playback (A2DP Sink) (sinks: 1, sources: 0, priority: 10, available: yes)
        off: Off (sinks: 0, sources: 0, priority: 0, available: yes)
Active Profile: a2dp_sink
Ports:
        headset-output: Headset (priority: 0, latency offset: 1250000 usec, available)
        Part of profile(s): headset_head_unit, a2dp_sink
        headset-input: Headset (priority: 0, latency offset: 0 usec)
        Part of profile(s): headset_head_unit‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Best regards,

Diego.

0 件の賞賛
返信
21,524件の閲覧回数
sergio_dorazio
Contributor IV

Hi Diego,

now I am working well with profile a2dp_sink, but for a requirement of my system I must work with HFP profile.

Activating only this profile I see the card, the sink and source interface but they not work. In some forum I read that HFP profile not work with bluez5 and than I need "oFono" application.

Do you now this configuration ? Can you send me a script sequence for work with oFono ? Or any link that help me ?

Regards.

Sergio.

0 件の賞賛
返信
21,524件の閲覧回数
sergio_dorazio
Contributor IV

Hi Diego,

now work not very well , but work. The audio quality is bad.

I have must add this command at my script:

hcitool cmd 0x3F 0x0210 0x01 120 511 0xFF

oFono isn't necessary.

Regard. Thank you for all.

By Sergio.

0 件の賞賛
返信
21,524件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

If you go to the /etc/pulse/daemon.conf where it says resample-method. Does equals to speex-float-3. If not, I suggest you change it to that.

Best regards,

Diego. 

0 件の賞賛
返信
21,524件の閲覧回数
sergio_dorazio
Contributor IV

Hi Diego, I put your suggest in file but the result isn't change.

I tell you what happen:

pulseaudio see 2 audio interface : local interface (imx6 board microphone and headset connected at audio connector) and bluetooth interface. Both are :

Sample Specification: s16le 1ch 8000Hz         Channel Map: mono

I want this configuration because I have customer specification.

Test 1 :

- on imx6 console play a .wav file on local interface

- on local headset the audio is perfect

Test 2 :

- on imx6 console play the same .wav file on bluetooth interface

- on remote bluetooth headset the audio is present but is very bad, incomprehensible words

Test 3:

-speak from remote bluetooth

-parecord on my imx6 test.wav

-paplay test.wav on bluetooth interface

-on the remote remote bluetooth I listen not very well but lissen, words comprehensible

-paplay test.wav on local interface

- on local headset the audio is present but is very bad, incomprehensible words

Test 4:

- make a loopback doing:

      pactl load-module module-loopback source=x sink=y latency_msec=10
      pactl load-module module-loopback source=z sink=k latency_msec=10

      (where x,y,z,k are pulseaudio name interface)

-speak from remote bluetooth

-on the local headset the audio is present but is very bad, incomprehensible words

Why ? Seems the analog and bluetooth have different type of interface.

Where do I make a mistake ?

Can you halp me ?

Sergio.

0 件の賞賛
返信
21,524件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

How are you attaching the UART connetion to the Bluez interface? Are you using hciattach? If yes, could you please pass me the command that you are using?

Best regards,

Diego.

0 件の賞賛
返信
21,524件の閲覧回数
sergio_dorazio
Contributor IV

My command is :

hciattach /dev/ttymxc1 texas 3000000

Sergio.

0 件の賞賛
返信
21,524件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Could you please try with.

hciattach /dev/ttymxc1 texas 3000000 flow -b -t 120

Best regards,

Diego.

0 件の賞賛
返信
21,524件の閲覧回数
sergio_dorazio
Contributor IV

I have test your command , but the result not change, I have the same problem.

I explain better :

with the following command I listen perfect on local board imx6 headset:

root@imx6ull14x14evk:~# paplay  -d alsa_output.platform-sound.analog-mono DataRe
layMode.wav -v
Opening a playback stream with sample specification 's16le 1ch 8000Hz' and channel map 'mono'.
Connection established.
Stream successfully created.
Buffer metrics: maxlength=4194304, tlength=32000, prebuf=31682, minreq=320
Using sample spec 's16le 1ch 8000Hz', channel map 'mono'.
Connected to device alsa_output.platform-sound.analog-mono (index: 0, suspended: no).
Stream started.
Stream underrun.
Playback stream drained.: 90221 usec.
Draining connection to server.

with the following command I listen bad on remote bluetooth headset:

root@imx6ull14x14evk:~# paplay  -d bluez_sink.BC_A5_8B_A3_8C_3A.headset_audio_ga
teway DataRelayMode.wav -v
Opening a playback stream with sample specification 's16le 1ch 8000Hz' and channel map 'mono'.
Connection established.
Stream successfully created.
Buffer metrics: maxlength=4194304, tlength=32000, prebuf=31682, minreq=320
Using sample spec 's16le 1ch 8000Hz', channel map 'mono'.
Connected to device bluez_sink.BC_A5_8B_A3_8C_3A.headset_audio_gateway (index: 1, suspended: no).
Stream started.
Playback stream drained.: 135550 usec.
Draining connection to server.
root@imx6ull14x14evk:~#

How you can see the duration of bluetooth play (Playback stream drained) is more then local interface, why ?

Infact the voice on headset bluetooth is low speed.

I hope that my play report help you to resolve the problem.

Sergio.

0 件の賞賛
返信
21,524件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Could you please try the following:

# pactl set-card-profile <Your Bluez card name or number> a2dp_sink

# pactl set-card-profile <Your Bluez card name or number> hsp_sink

# pactl set-card-profile <Your Bluez card name or number> a2dp_sink

If that doesn't work. Please modify the resample method on the /etc/pulse/daemon.conf to trivial. Don´t forget to restart the pulseaudio service.

# pulseaudio -k

Hope this could solve your problem.

Best regards,

Diego.

0 件の賞賛
返信
21,524件の閲覧回数
sergio_dorazio
Contributor IV

Hi Diego,

bad news:

when I put your command I have this error:

root@imx6ull14x14evk:~# pactl set-card-profile bluez_sink.BC_A5_8B_A3_8C_3A.head
set_audio_gateway  a2dp_sink
Failure: No such entity

My card is :

Card #1
Name: bluez_card.BC_A5_8B_A3_8C_3A
Driver: module-bluez5-device.c
Owner Module: 20
Properties:
device.description = "SDO Galaxy J6"
device.string = "BC:A5:8B:A3:8C:3A"
device.api = "bluez"
device.class = "sound"
device.bus = "bluetooth"
device.form_factor = "phone"
bluez.path = "/org/bluez/hci0/dev_BC_A5_8B_A3_8C_3A"
bluez.class = "0x5a020c"
bluez.alias = "SDO Galaxy J6"
device.icon_name = "audio-card-bluetooth"
Profiles:
a2dp_source: High Fidelity Capture (A2DP Source) (sinks: 0, sources: 1, priority: 10, availabl
e: no)
headset_audio_gateway: Headset Audio Gateway (HSP/HFP) (sinks: 1, sources: 1, priority: 20, av
ailable: yes)
off: Off (sinks: 0, sources: 0, priority: 0, available: yes)
Active Profile: off
Ports:
phone-output: Phone (priority: 0, latency offset: 0 usec)
Part of profile(s): headset_audio_gateway
phone-input: Phone (priority: 0, latency offset: 0 usec)
Part of profile(s): a2dp_source, headset_audio_gateway

I don't know why I have error !!!!! The card name is correct, if I put the number I have the same error.

Then I try the second test modify /etc/pulse/daemon.conf , I don't have errors but the output audio on bluetooth terminal is null. In the file now I have  "resample-method = speex-float-3". What is the correct resample-method for HFP bluetooth stream with sample specification 's16le 1ch 8000Hz' and channel map 'mono' ?

In the card I have "headset_audio_gateway" profile , is it correct for my configuration ?

Sergio.

0 件の賞賛
返信
21,525件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

In the card name try without the headset_audio_gateway. Just write: 

# pactl set-card-profile bluez_sink.BC_A5_8B_A3_8C_3A a2dp_sink

Or

# pactl set-card-profile 1 a2dp_sink

Both options should work.

Best regards,

Diego.

0 件の賞賛
返信
21,524件の閲覧回数
sergio_dorazio
Contributor IV

Hello Diego,

on my board the command

# pactl set-card-profile 1 a2dp_sink

not work, the only command that work is :

# pactl set-card-profile 1 off

so it means that the parameter '1' is ok .

What is your suggestion now ?

Could my bluetooth chip need a special command like 'hcitool cmd xx xx xx xx xx' ?

Sergio.

0 件の賞賛
返信
21,525件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

I do not know if the problem is the Bluetooth device that you are trying to set a connection. I have read that the newest version of Bluez has some problems with some Bluetooth devices. Could you please test with another device?

Best regards,

Diego.

0 件の賞賛
返信
21,525件の閲覧回数
sergio_dorazio
Contributor IV

Hi Diego,

for the moment I cannot test with another device.

Now I go on in two ways:

  1. put some trace to see where is the problem.
  2. study the script sequence if it is correct

Can you have other suggestion ?

Sergio.

0 件の賞賛
返信
21,510件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

I apologize for the delay. I suggest you put a trace to see the problem.

I am testing with bluez with the QCA Bluetooth module using the suggestions that I already made and the Bluetooth connection worked without a problem. Your problem seems to be related that your bluez audio card is not being recognized as an a2dp_sink source.

Best regards,

Diego.

21,682件の閲覧回数
sergio_dorazio
Contributor IV

Hi Diego,

The problem is the mtu dimension of my BT chip, it is 180 bytes.

I have solved the problem putting in /etc/pulse/default.pa this line

load-module module-bluetooth-discover autodetect_mtu=yes

and modifing the file backend-ofono.c , in the pulseaudio yocto module , the fixed mtu from 48 to 180.

(in this file there isn't autodetect_mtu manage and than I have fixed value set).

By.

Sergio.