pull-up/pull-down resistors's tolerance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pull-up/pull-down resistors's tolerance

Jump to solution
3,956 Views
ko-hey
Senior Contributor II

Hi all

I have a question about resistance tolerance.

I want to know the resistance tolerance of GPIO's pull-up/pull-down resistors.

I can't find it in section 4.6.2 of following datasheet.

http://cache.nxp.com/files/32bit/doc/data_sheet/IMX6SDLIEC.pdf

Please provide the spec.

ko-hey

Labels (1)
0 Kudos
Reply
1 Solution
3,799 Views
art
NXP Employee
NXP Employee

The tolerance of the i.MX6 series internal pull-up/down I/O resistors is +/- 10%.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
3,800 Views
art
NXP Employee
NXP Employee

The tolerance of the i.MX6 series internal pull-up/down I/O resistors is +/- 10%.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,799 Views
ko-hey
Senior Contributor II

Is the data described somewhere in RM ?

Ko-hey

0 Kudos
Reply