pslash on multiple displays

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

pslash on multiple displays

2,441 次查看
andreykononov
Contributor III

I'm using sabreai in my project and connect 3 displays on it (2*LVDS+HDMI). When board starting, psplash show picture only on main screen, is it posible to show same or other picture on other monitors?

PS:

board: Sabre AI I.MX6QP

Os: # uname -a
Linux MMC 4.1.15-2.0.0+gb63f3f5 #5 SMP PREEMPT Tue Mar 14 10:59:16 MSK 2017 armv7l armv7l armv7l GNU/Linux

0 项奖励
回复
3 回复数

2,285 次查看
claymontgomery
Contributor IV

The FBDEV environment variable controls which display receives the output graphics from psplash. You could modify psplash-fb.c to replicate the images on all the displays.

  fbdev = getenv("FBDEV");
  if (fbdev == NULL)
    fbdev = "/dev/fb0";

Regards, Clay

2,285 次查看
andreykononov
Contributor III

very interesting, i'l try

0 项奖励
回复

2,285 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Andrey,

Never tried on three display, however If you are using 2 LVDS displays then there is a dual-mode setting in the LDB which clones the data from one display to other.

To enable it you will have to add the 'dual-mode' property in LDB's device tree node.

hope this helps

0 项奖励
回复