processor can share the same external flash memory?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

processor can share the same external flash memory?

1,772件の閲覧回数
mohammed_saleh
Contributor I

In one of our RFQ, We are using MIMX8MN2DVTJZAA as the primary processor and MIMXRT1051DVJ6B  from NXP USA Inc as to the secondary processor.

Can you please help us to solve below query?

 

Whether two processor can share the same external flash memory?

0 件の賞賛
返信
1 返信

1,719件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mohammed

in general - no, as these processors have not special modules for sharing memory.

One can consider using i2c or spi nor dual port chips, if such avaialble.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信