processing limit of CAAM hardware?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

processing limit of CAAM hardware?

1,280件の閲覧回数
gbiradar
Contributor IV

Hi Guys,

              i'm cryptodev engine to encrypt data so i want to know what is the maximum amount of data size can caam process. say i want to encrypt streaming data of high definition video.

thanks

Ganesh

ラベル(5)
0 件の賞賛
返信
1 返信

1,137件の閲覧回数
bpe
NXP Employee
NXP Employee

This question is a bit vague. There is no global limit to the data

amount processed by CAAM. With a single descriptor, however, the

number of bytes that can be processed is limited by the size of the

LENGTH field of FIFO LOAD/FIFO STORE command, which is 16 bits. Some cipher modes,

namely counter-based, require a re-key after certain amount of processed

data to stay secure. This is, however, not a CAAM limitation.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信