problem with meta-toolchain in imx6 sololite

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

problem with meta-toolchain in imx6 sololite

1,454 次查看
susangracerapak
Contributor II

hello,

iam working with imx6 sololite(yocto project).

firstly,i downloaded the source code for 3.10.17 kernel.then i did bitbake core-image-minimal.It's booting successfully.

then, i did bitbake meta-toolchain for toolchain.i got this error....please let me know how to fix it.

thank you

susan@susan:/imx6_sololite/fsl-release-bsp/build$ bitbake meta-toolchain

Loading cache: 100% |########################################################################################################################################################################| ETA:  00:00:00

Loaded 2005 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION        = "1.20.0"

BUILD_SYS         = "i686-linux"

NATIVELSBSTRING   = "Ubuntu-12.04"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "imx6slevk"

DISTRO            = "poky"

DISTRO_VERSION    = "1.5.1"

TUNE_FEATURES     = "armv7a vfp neon callconvention-hard cortexa9"

TARGET_FPU        = "vfp-neon"

meta             

meta-yocto        = "(nobranch):bee7e3756adf70edaeabe9d43166707aab84f581"

meta-oe           = "(nobranch):eb4563b83be0a57ede4269ab19688af6baa62cd2"

meta-fsl-arm      = "(nobranch):af392c22bf6b563525ede4a81b6755ff1dd2c1c6"

meta-fsl-arm-extra = "(nobranch):07ad83db0fb67c5023bd627a61efb7f474c52622"

meta-fsl-demos    = "(nobranch):5a12677ad000a926d23c444266722a778ea228a7"

meta-fsl-arm     

meta-fsl-demos    = "(nobranch):fd639897114c09d5146ea1399c16308edfd0108b"

meta-browser      = "(nobranch):fc3969f63bda343c38c40a23f746c560c4735f3e"

meta-gnome       

meta-networking   = "(nobranch):eb4563b83be0a57ede4269ab19688af6baa62cd2"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

WARNING: Failed to fetch URL http://downloads.sourceforge.net/project/libpng/libpng16/1.6.3/libpng-1.6.3.tar.xz, attempting MIRRORS if available

WARNING: QA Issue: gcc-cross-canadian-arm: found library in wrong location: /opt/poky/1.5.1/sysroots/i686-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.8.1/liblto_plugin.so.0

gcc-cross-canadian-arm: found library in wrong location: /opt/poky/1.5.1/sysroots/i686-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.8.1/liblto_plugin.so.0.0.0

gcc-cross-canadian-arm: found library in wrong location: /opt/poky/1.5.1/sysroots/i686-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.8.1/liblto_plugin.so

标签 (4)
0 项奖励
回复
1 回复

854 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Susangrace Rapaka,

The log does not show any error. It does show a fetch warning. Would you please add the information regarding the encountered error?

0 项奖励
回复