problem with build obds project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem with build obds project

Jump to solution
2,439 Views
caoping
Contributor II

Hi,everyone

now i want to have one test project on my computer to test the imx53 board,  i install the Ubuntu 10.04

according to "README_Ubuntu_VM.pdf",

when i run "cat /proc/version",it displays

Linux version 2.6.32-21-generic (buildd@rothera) (gcc version 4.4.3 (Ubuntu 4.4.3-4ubuntu5) ) #32-Ubuntu SMP

Fri Apr 16 08:10:02 UTC 2010

and then i download "I201139_mx53_sbrth_lcb_release" on freescale webside,and

coye"I201139_mx53_sbrth_lcb_release" to ubuntu "Desktop",and change I201139_mx53_sbrth_lcb_release's name

into obds,in the path /Desktop/obds,when i run"make TARGET=mx53 BOARD=sbrth_lcb BOARD_VERSION=1",it displays

mkdir -p output

mkdir -p output/mx53

mkdir -p /home/lucid/Desktop/obds/output/mx53/lib

mkdir -p /home/lucid/Desktop/obds/output/mx53/bin

make -S -C src dir

make[1]: Entering directory `/home/lucid/Desktop/obds/src'

make -S -C drivers dir

make[2]: Entering directory `/home/lucid/Desktop/obds/src/drivers'

make -S -C usb dir

make[3]: Entering directory `/home/lucid/Desktop/obds/src/drivers/usb'

make -S -C imx_usb dir

make[4]: Entering directory `/home/lucid/Desktop/obds/src/drivers/usb/imx_usb'

arm-none-eabi-ar -rucs /home/lucid/Desktop/obds/output/mx53/lib/libobds.a

/home/lucid/Desktop/obds/output/mx53/obj/imx_usb/usb_h1.o

/home/lucid/Desktop/obds/output/mx53/obj/imx_usb/usb_test.o

make[4]: arm-none-eabi-ar: Command not found

make[4]: *** [all] Error 127

make[4]: Leaving directory `/home/lucid/Desktop/obds/src/drivers/usb/imx_usb'

make[3]: *** [imx_usb] Error 2

make[3]: Leaving directory `/home/lucid/Desktop/obds/src/drivers/usb'

make[2]: *** [usb] Error 2

make[2]: Leaving directory `/home/lucid/Desktop/obds/src/drivers'

make[1]: *** [drivers] Error 2

make[1]: Leaving directory `/home/lucid/Desktop/obds/src'

make: *** [src] Error 2

and when i change

CC= arm-none-eabi-gcc

AS = arm-none-eabi-as

AR = arm-none-eabi-ar

LN = arm-none-eabi-ld

into

CC = /opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-fsl-linux-gnueabi-gcc

AS = /opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-fsl-linux-gnueabi-as

AR = /opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-fsl-linux-gnueabi-ar

LN = /opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-fsl-linux-gnueabi-ld

and run "make TARGET=mx53 BOARD=sbrth_lcb BOARD_VERSION=1",it displays

/home/lucid/Desktop/obds/src/init/sys.c:137: warning: its scope is only this definition or declaration,

which is probably not what you want

/home/lucid/Desktop/obds/src/init/sys.c: In function '_write':

/home/lucid/Desktop/obds/src/init/sys.c:183: warning: null argument where non-null required (argument 2)

/home/lucid/Desktop/obds/src/init/sys.c:186: warning: null argument where non-null required (argument 2)

collect2: ld terminated with signal 11 [Segmentation fault]

/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/../lib/gcc/arm-fsl-

linux-gnueabi/4.4.4/../../../../arm-fsl-linux-gnueabi/bin/ld: BFD (GNU Binutils) 2.20.1.20100303 assertion

fail /work/arm-toolchains/tmp/src/binutils-2.20.1/bfd/elf32-arm.c:12429

make: *** [bin] Error 1

how can i compile the project,can anyone use it?


Labels (1)
0 Kudos
Reply
1 Solution
1,796 Views
Yuri
NXP Employee
NXP Employee

Please use CodeSourcery (Mentor) toolchain (under Linux host) for stand-alone applications :
arm-none-gnueabi-gcc.

SOURCERY CODEBENCH LITE

http://www.mentor.com/embedded-software/codesourcery

View solution in original post

0 Kudos
Reply
3 Replies
1,797 Views
Yuri
NXP Employee
NXP Employee

Please use CodeSourcery (Mentor) toolchain (under Linux host) for stand-alone applications :
arm-none-gnueabi-gcc.

SOURCERY CODEBENCH LITE

http://www.mentor.com/embedded-software/codesourcery

0 Kudos
Reply
1,796 Views
caoping
Contributor II

hi, when i install the project,and excute

PATH=installdir/bin:$PATH

export PATH

and excute:make TARGET=mx53 BOARD=sbrth_lcb BOARD_VERSION=1

then it complete successfully.

0 Kudos
Reply
1,796 Views
caoping
Contributor II

hi thank you for you reply,i have downloaded the software,but i'm not familiar with it,do you have any existing project of OBDS that runs in the "SOURCERY CODEBENCH LITE" development environment.

0 Kudos
Reply