problem setting Horizontal Sync Width and Pixel Clock Cycle Frequency on IMX51

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem setting Horizontal Sync Width and Pixel Clock Cycle Frequency on IMX51

1,905件の閲覧回数
FrancescoPapa
Contributor I

Hi,

I'm using an LVDS LG display  LP097X02-SLQ1 with a custom imx51 board with CE6.

I set the parameters of the display in the file panels.h on C:\WINCE600\PLATFORM\iCoreM51bsp\SRC\DRIVERS\IPUV3\DISPLAY

I've to set Horizontal Sync Width to 320 Pixel Clock Cycle and a Pixel Clock Cycle Frequency of 100mhz.

Setting it also independently, Horizontal Sync Width run until 255 while other value as Horizontal Start Width runs at 480 also, moreover the frequency doesnt work correctly (i copy the frequency parameter from DVI SXGA Panel into the file).

Could anyone help?

Thanks in Advance

Regards

Francesco

 

 

タグ(2)
3 返答(返信)

1,548件の閲覧回数
YixingKong
Senior Contributor IV

Frances

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 件の賞賛
返信

1,548件の閲覧回数
YixingKong
Senior Contributor IV

Francesco

We have not got your response yet and will close the diacussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信

1,548件の閲覧回数
YixingKong
Senior Contributor IV

Francesco

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need Freescale help, please feel free to contact us.

Thanks,

Yixing

0 件の賞賛
返信