problem running bin file from u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem running bin file from u-boot

1,995 Views
saida
Contributor II

hi

this is saida

wordking on custmoised i.mx6 board 

i am using ARM DS5 and Dstream for code development,debugging respectively

i am facing one problem

i have one application code which running with debugger perfectly but 

the same bin file when i am running from u-boot with loadb command

its not running and it is going to SVC,UNDEF,ABORT handlers

the code is given below

/*******************************************/

struct t1
{
float x;
int y;
};
typedef struct t1 t1struct;

struct six
{
float xx;
int yy;
t1struct xyz;
boolean v;
};
typedef struct six sixstruct;

void datacopy(t1struct *T)
{
T->y =1;
}
void start(sixstruct *data)
{
datacopy(&(data->xyz));
}

int main(void)
{
sixstruct s;
start(&s);

return EXIT_SUCCESS;
}

/******************************************/

please can any one help me in this regard

thanks in advance

regards

Saida

Labels (1)
0 Kudos
Reply
2 Replies

1,911 Views
igorpadykov
NXP Employee
NXP Employee

Hi Saida

one can look at map file to find correct "main" address and run from

that address. More hints can be found on:

https://community.nxp.com/thread/359068 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,911 Views
saida
Contributor II

thank you for your reply

i am using startup.s file which i found in ds5 archieves

i am running so many applications from same memory address

my scatter file address is 0x20000000

while debugging

i am observed that when calling this routine datacopy(&(data->xyz));

then it is aborted

if i comment all this kind of function calling then it is working

i have done small test also

just used this test code

struct rt

{   int x;

float y;

}

typedef struct rt rtstruct;

rtstruct *ptr

if i call ptr->x

then also it is aborting

it is somthing pointer and structure formation problem

it is giving memory aborts

if possible can you try in ds5 and run it

from this community i have learned more and  solved few issues also

i hope i can solve this problem with all your help

i thank all the people who are supported me

regards

saida

0 Kudos
Reply