problem of I.MX6 otg identify

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem of I.MX6 otg identify

922 Views
sharpjison
Contributor II

I'm using i.MX6 q4 OTG, system: linux, kernel version: 3.0.35 .

I found a problem that the OTG host mode can not be identified after the device boot up;

when booting the linux kernel , I insert the Micro USB cable(let the ID pin level low) the OTG host mode can be idenfied correctly;

Labels (3)
0 Kudos
Reply
1 Reply

854 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sharp

one can check if usb_id signal is grouned and test with unit

tests package (folder /mxc_usb_test)

Index of /buildsources/i/imx-test/imx-test-3.0.35-4.0.0 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply