Hi
I was trying to create a new layer using this great thread by Daiane Angolini which works for the test program (helloworld).
but when I'm trying to create a simple library file and install it, I face with a problem.
here's the structure:
meta-sample-c-library/
├── conf
│ └── layer.conf
├── COPYING.MIT
├── README
└── recipes-example
└── example
├── newClibrary-0.1
│ └── foo1.c
└── newClibrary_0.1.bb
which I added to the bblayer config file.
now
bitbake newClibrary
succeeds.
Then I added the result to local.conf file:
CORE_IMAGE_EXTRA_INSTALL += "newClibrary"
but building the final image fails:
bitbake core-image-minimal
here's the error I get:
Error: newClibrary not found in the base feeds (nitrogen6x cortexa9hf-vfp-neon-mx6 cortexa9hf-vfp-neon cortexa9hf-vfp armv7ahf-vfp-neon armv7ahf-vfp armv6hf-vfp armv5ehf-vfp armv5hf-vfp noarch any all).
here's also the newClibrary recipe:
DESCRIPTION = "Simple helloworld application"
SECTION = "examples"
LICENSE = "CLOSED"
PR = "r0"
SRC_URI = "file://foo1.c"
S = "${WORKDIR}"
do_compile() {
${CC} -c foo1.c -o foo.o
${AR} rcs libfoo1.a foo.o
}
do_install() {
install -d ${D}${libdir}
install -m 0755 libfoo1.a ${D}${libdir}
}
Any suggestions about what's the problem?
(I also attached all the files)
Thanks,
Mahyar
Original Attachment has been moved to: meta-sample-c-library.tar.gz