problem in port the mag3110 driver to linux source code for imx53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem in port the mag3110 driver to linux source code for imx53

Jump to solution
3,560 Views
ehsanrezaie
Contributor I

i'm tring to port mag3110 to imx 53 qsb board by drivers that

presented with this property(downloaded from freescale website):

 

 

/******************** (C) COPYRIGHT 2012 Freescale Semiconductor, Inc.

 

   * File Name            : mag_3110.c
* Authors              : Rick Zhang([email protected]

 

)
                          Rick is willing to be considered the contact and update points
                          for the driver
* Version              : V.1.0.0
* Date                 : 2012/Mar/15
* Description          : methods and data structure related to MAG3110
magnetometer sensor.
   ******************************************************************************

 

          *******************************************************************
* Revision 1.0.0 3/15/2012 First Release;
******************************************************************************

 

 

and i try to port with readme sequence and using ltib(install from freescaleL2.6.35_11_09_ER_SOURCE package)   .

 

but in step 5 of readme sequence(Configure and compile the driver)i have problem in complie ):

 

 

 

 

--------------------------------
drivers/hwmon/mag3110/mag_core.c:44:31: error: linux/fsl_sensors.h: No
such file or directory
In file included from drivers/hwmon/mag3110/mag_core.c:46:
drivers/hwmon/mag3110/mag_regs.h:33:28: error: linux/wakelock.h: No
such file or directory

-------------------------------------------------

 

so , how i can solve this problem?  .

i attached read me file & complete compile error report


i cant find header files like wakelock.h on the internet.

Original Attachment has been moved to: mag_3110.c.zip

Original Attachment has been moved to: Readme.txt.zip

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
3,302 Views
jimmychan
NXP TechSupport
NXP TechSupport

there are some difference between Android linux kernel and linux standard kernel, please try to use attachment file to replace the old one.

View solution in original post

0 Kudos
Reply
2 Replies
3,303 Views
jimmychan
NXP TechSupport
NXP TechSupport

there are some difference between Android linux kernel and linux standard kernel, please try to use attachment file to replace the old one.

0 Kudos
Reply
3,302 Views
bottleneck
Contributor II

Could you help me in sharing the pad and mux configuration and i2c frequency divider register values for SABRESD board. I am not getting acknowledge from the device.

Please do needful

0 Kudos
Reply