i.MX6 HDMI pixel repeater.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 HDMI pixel repeater.

Jump to solution
1,066 Views
satoshishimoda
Senior Contributor I

Hi community,

We have a question about i.MX6 HDMI.

Please see Figure 34-6 in IMX6SDLRM Rev.1.

There is "Pixel Repeater" in this figure, but we did not find the description of this block.

So would you let me know the detail of "Pixel Repeater"?

Best Regards,

Satoshi Shimoda

Tags (1)
0 Kudos
Reply
1 Solution
676 Views
Yuri
NXP Employee
NXP Employee

  "Audio, video, and auxiliary data is transmitted across the three TMDS data channels.

Video formats with TMDS rates below 25MHz (such as, 13.5MHz for 480i/NTSC)

can be transmitted using a pixel-repetition scheme."

  "HDMI_TX can output video in full HD with up to 48-bit color mode and inserts

high fidelity audio up to eight-channels over low resolution video formats by performing

automatic pixel repetition over the input video stream."
  From HDMI specs:
"Pixel Repetition
During pixel-doubling (Pixel_Repetition_Count = 1), all of the data sent across during the
first pixel period will be repeated during the second pixel period. The third pixel period will

then represent the second actual pixel and so on".

  There are no more details about the Pixel Repeater, sorry.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
677 Views
Yuri
NXP Employee
NXP Employee

  "Audio, video, and auxiliary data is transmitted across the three TMDS data channels.

Video formats with TMDS rates below 25MHz (such as, 13.5MHz for 480i/NTSC)

can be transmitted using a pixel-repetition scheme."

  "HDMI_TX can output video in full HD with up to 48-bit color mode and inserts

high fidelity audio up to eight-channels over low resolution video formats by performing

automatic pixel repetition over the input video stream."
  From HDMI specs:
"Pixel Repetition
During pixel-doubling (Pixel_Repetition_Count = 1), all of the data sent across during the
first pixel period will be repeated during the second pixel period. The third pixel period will

then represent the second actual pixel and so on".

  There are no more details about the Pixel Repeater, sorry.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply