problem in accessing rfs from /dev/mtdblock4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem in accessing rfs from /dev/mtdblock4

1,809件の閲覧回数
parthahazra
Contributor I

I am trying to mount my file system jffs2 from Nor flash (WEIM Bus) in linux 3.7-rc4.

I am able to access NOR flash from uboot and write the images at partitions mentioned in below log.

Following command is used to build a jffs2 image.

mkfs.jffs2 -e 128 -l -n -r rootfs -v -o test.jffs2

File system fails to  boot after kernel has come up.

Please refer to the below error log.

Please suggest.

jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

fuse init (API version 7.20)

msgmni has been set to 3525

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

imx-sdma 20ec000.sdma: initialized

Serial: IMX driver

21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61) is a IMX

console [ttymxc3] enabled

brd: module loaded

loop: module loaded

8000000.nor_flash: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000001 Chip ID 0x002801

NOR chip too large to fit in mapping. Attempting to cope...

Amd/Fujitsu Extended Query Table at 0x0040

  Amd/Fujitsu Extended Query version 1.5.

number of CFI chips: 1

Reducing visibility of 131072KiB chip to 64512KiB

7 ofpart partitions found on MTD device 8000000.nor_flash

Creating 7 MTD partitions on "8000000.nor_flash":

0x000000000000-0x000000080000 : "bootloader"

0x000000080000-0x0000000a0000 : "environment"

0x0000000a0000-0x0000000c0000 : "redundant-environment"

0x0000000c0000-0x0000004c0000 : "kernel"

0x0000004c0000-0x000002cc0000 : "filesystem"

0x000002cc0000-0x000002ce0000 : "devicetree"

0x000002ce0000-0x0000036e0000 : "user_space"

mousedev: PS/2 mouse device common for all mice

i2c /dev entries driver

TCP: cubic registered

NET: Registered protocol family 17

NET: Registered protocol family 33

Key type rxrpc registered

Key type rxrpc_s registered

Key type dns_resolver registered

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

drivers/rtc/hctosys.c: unable to open rtc device (rtc0)

jffs2: jffs2_scan_eraseblock(): Node at 0x00000000 {0x1985, 0xe001, 0x0000002b) has invalid CRC 0x7d266ce6 (calculated 0x7d266ee6)

jffs2: jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000004: 0x002b instead

jffs2: jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000008: 0x6ce6 instead

jffs2: jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x0000000c: 0x0001 instead

jffs2: jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000014: 0x0002 instead

jffs2: jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000018: 0x5192 instead

jffs2: jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x0000001c: 0x0403 instead

jffs2: jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000020: 0x10a3 instead

jffs2: jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000024: 0x81ff instead

jffs2: jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000028: 0x6962 instead

ラベル(1)
0 件の賞賛
返信
0 返答(返信)