problem from resizing Ubuntu.vmx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem from resizing Ubuntu.vmx

2,037件の閲覧回数
HuiShao
Contributor I

Working under virtual machine shipped with QSB DVD, virtual hardisk file Ubuntu.vmx quickly was ran out of disk space. Tried to resize the harddisk space by "virtual machin settings -> harddisk -> utilities -> expand" and got 20G more space in guest OS Ubuntu. However, after partition and formating it into ext4, it turns into READ ONLY after mount command.

 

What I did is:

$sudo mount -t ext4 /dev/sda3 /home/lucid/work

 

Plus if I go to modify /etc/mtab to add one more line similar to "/dev/sda1", it is gone after reboot.

 

Can anybody help on that? I would be ideal if I can re-size root partition directly.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,973件の閲覧回数
HuiShao
Contributor I

thanks! Guys.

 

I have to change onwership of /home/lucid/work from root to lucid by

sudo chown lucid:lucid /home/lucid/work

 

Then it ends up writtable.

0 件の賞賛
返信

1,973件の閲覧回数
Yuri
NXP Employee
NXP Employee

You may to to use option remount :

mount -o remount,rw /dev/sda1 /home/lucid/work

0 件の賞賛
返信

1,973件の閲覧回数
PaulRobertson
Contributor I

I have not tried this.  So you will understand these "offerings" are just brainstorming:

   1) Although read/write is supposed to be the default, it seems possible you could add the -w option (or -o rw).

   2) Check the mode/owner of the directory /home/lucid/work and make sure that isn't set to preclude writing.

hth,

pr

0 件の賞賛
返信