problem about eim mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem about eim mode

1,294 Views
vvjay
Contributor I

Hi,    

   we have succeed in eim multiplexed mode , but for some reason we have to use eim non-multiplexed mode. we use csi camera ,so csi0 pins can not be used as eim_data[0:15] , so for data bus ,we have not choice but use eim_data[16:31]. But i find that some of those pads are use for usb otg and usb otg is used to flash uImage ,fs and so on. Does it influence eim data bus if we dont change configure because after flash we do not use usb otg any more, or does it mean that  we have to disable usb otg after we flashed uImage? i can not try it now, so i have to ask anyone who know the answer.

Thank you!

Jay

Labels (1)
0 Kudos
Reply
1 Reply

1,215 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wenjie

if iomux settings configured in such way that usb

does not interference with eim, then usb (or other module)

may be not disabled.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply