print_req_error: I/O error, dev mmcblk2rpmb, sector 0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

print_req_error: I/O error, dev mmcblk2rpmb, sector 0

2,365件の閲覧回数
Andre123
Contributor I

Hi, 

Kernel version:

Linux myd-imx8mm 4.14.98-myd-imx8mm-dev-v14+g940c0ea #1 SMP PREEMPT Mon Nov 8 08:22:14 UTC 2021 aarch64 aarch64 aarch64 GNU/Linux

Processor:

NXP i.MX8M Mini

If the following error message is displayed after the fdisk -l command is executed in the system, how can I solve the problem:

root@myd-imx8mm:~# fdisk -l
Disk /dev/mtdblock0: 32 MiB, 33554432 bytes, 65536 sectors
33.245334] mmc2: running CQE recovery
[0mUnits: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes


Disk /dev/mmcblk2: 7.3 GiB, 7818182656 bytes, 15269888 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disklabel type: dos
Disk identifier: 0x98888df1

Device End Sectors Size Id Type
/dev/mmcblk2p1 20480 1044479 1024000 500M c W95 FAT32 (LBA)
/dev/mmcblk2p2 1228800 15269887 14041088 6.7G 83 Linux


[ 33.351909] mmc2: running CQE recovery
[ 33.355771] mmc2: running CQE recovery
[ 33.359592] print_req_error: I/O error, dev mmcblk2rpmb, sector 0
[ 33.365922] mmc2: running CQE recovery
[ 33.369788] mmc2: running CQE recovery
[ 33.373628] mmc2: running CQE recovery
[ 33.377478] print_req_error: I/O error, dev mmcblk2rpmb, sector 0
[ 33.383606] Buffer I/O error on dev mmcblk2rpmb, logical block 0, async page read
[ 33.391276] mmc2: running CQE recovery
[ 33.395181] mmc2: running CQE recovery
[ 33.399045] mmc2: running CQE recovery
[ 33.402870] print_req_error: I/O error, dev mmcblk2rpmb, sector 0
[ 33.408999] Buffer I/O error on dev mmcblk2rpmb, logical block 0, async page read


Disk /dev/mmcblk2boot1: 4 MiB, 4194304 bytes, 8192 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes


Disk /dev/mmcblk2boot0: 4 MiB, 4194304 bytes, 8192 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes

 

 

 

0 件の賞賛
返信
1 返信

2,340件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Erase and burn again the sdcard or Change it, loss like is damage.

Regards

0 件の賞賛
返信