prebuilt image for sabresd board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

prebuilt image for sabresd board

3,643件の閲覧回数
sachusanal
Contributor III

Hai Sir ,

Could you please provide one ubuntu(yocto) prebuilt image for IMX6Q Sabresd board.

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

3,066件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sachu

FSL Demo :

Board Support Packages (27)

L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

Yocto Community Demo:

http://blink.ossystems.com.br/#/

http://blink.ossystems.com.br/#/boards/imx6qsabresd?p=4

Best regards

igor

0 件の賞賛
返信

3,065件の閲覧回数
sachusanal
Contributor III

Could u please share me the imx6q sabresd board prebuilt image which is providedi from freescale at the time of board purchasing.

please give me exact link to download the prebuilt image for yocto

please help me , its urgent task

0 件の賞賛
返信

3,065件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

please use prebuilt images:

FSL Demo :

Board Support Packages (27)

L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

0 件の賞賛
返信

3,066件の閲覧回数
sachusanal
Contributor III


I couldn't find out this image ( L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0) ) in the above mentioned site. please help me .....

it's urgent task

0 件の賞賛
返信

3,066件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

3,066件の閲覧回数
sachusanal
Contributor III

Hai ,

Thnaks for your support.I flashed the image .

Actually i need the image which all package enabled prebuilt image which is given at the board purchasing time.

in the above image qt is working but apt-get command is not working . I need these all command working image

0 件の賞賛
返信

3,066件の閲覧回数
saurabh_patel
NXP Pro Support
NXP Pro Support

Hi

Sachu

You can build yocto using following steps

Yocto Training - HOME

Saurabh

0 件の賞賛
返信