prebuilt image for sabresd board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

prebuilt image for sabresd board

2,840 Views
sachusanal
Contributor III

Hai Sir ,

Could you please provide one ubuntu(yocto) prebuilt image for IMX6Q Sabresd board.

Labels (1)
0 Kudos
Reply
7 Replies

2,263 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sachu

FSL Demo :

Board Support Packages (27)

L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

Yocto Community Demo:

http://blink.ossystems.com.br/#/

http://blink.ossystems.com.br/#/boards/imx6qsabresd?p=4

Best regards

igor

0 Kudos
Reply

2,262 Views
sachusanal
Contributor III

Could u please share me the imx6q sabresd board prebuilt image which is providedi from freescale at the time of board purchasing.

please give me exact link to download the prebuilt image for yocto

please help me , its urgent task

0 Kudos
Reply

2,262 Views
igorpadykov
NXP Employee
NXP Employee

please use prebuilt images:

FSL Demo :

Board Support Packages (27)

L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

0 Kudos
Reply

2,263 Views
sachusanal
Contributor III


I couldn't find out this image ( L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0) ) in the above mentioned site. please help me .....

it's urgent task

0 Kudos
Reply

2,263 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

2,263 Views
sachusanal
Contributor III

Hai ,

Thnaks for your support.I flashed the image .

Actually i need the image which all package enabled prebuilt image which is given at the board purchasing time.

in the above image qt is working but apt-get command is not working . I need these all command working image

0 Kudos
Reply

2,263 Views
saurabh_patel
NXP Pro Support
NXP Pro Support

Hi

Sachu

You can build yocto using following steps

Yocto Training - HOME

Saurabh

0 Kudos
Reply