porting of OPEN GL drivers for imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

porting of OPEN GL drivers for imx6

跳至解决方案
1,637 次查看
Deepu
Contributor III

since I am working on porting of OPENGL drivers for imx6 boards. Can anyone tell me where these driver sources are available.I need to port OPENGL drivers to imx6 which is not using any windowing system (X serve) but with frame buffer support.

标记 (2)
0 项奖励
回复
1 解答
926 次查看
claymontgomery
Contributor IV

Freescale does not make the source code of their OpenGL ES drivers available.  None of the embedded chip vendors provide that.  Also, the 3D Core in i.MX6 series is different than for the i.MX5x series.  It is Vivante instead of AMD, so the new OpenGL ES drivers were developed by Vivante.

在原帖中查看解决方案

0 项奖励
回复
1 回复
927 次查看
claymontgomery
Contributor IV

Freescale does not make the source code of their OpenGL ES drivers available.  None of the embedded chip vendors provide that.  Also, the 3D Core in i.MX6 series is different than for the i.MX5x series.  It is Vivante instead of AMD, so the new OpenGL ES drivers were developed by Vivante.

0 项奖励
回复