since I am working on porting of OPENGL drivers for imx6 boards. Can anyone tell me where these driver sources are available.I need to port OPENGL drivers to imx6 which is not using any windowing system (X serve) but with frame buffer support.
Solved! Go to Solution.
Freescale does not make the source code of their OpenGL ES drivers available. None of the embedded chip vendors provide that. Also, the 3D Core in i.MX6 series is different than for the i.MX5x series. It is Vivante instead of AMD, so the new OpenGL ES drivers were developed by Vivante.
Freescale does not make the source code of their OpenGL ES drivers available. None of the embedded chip vendors provide that. Also, the 3D Core in i.MX6 series is different than for the i.MX5x series. It is Vivante instead of AMD, so the new OpenGL ES drivers were developed by Vivante.