porting of OPEN GL drivers for imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

porting of OPEN GL drivers for imx6

Jump to solution
1,563 Views
Deepu
Contributor III

since I am working on porting of OPENGL drivers for imx6 boards. Can anyone tell me where these driver sources are available.I need to port OPENGL drivers to imx6 which is not using any windowing system (X serve) but with frame buffer support.

0 Kudos
Reply
1 Solution
852 Views
claymontgomery
Contributor IV

Freescale does not make the source code of their OpenGL ES drivers available.  None of the embedded chip vendors provide that.  Also, the 3D Core in i.MX6 series is different than for the i.MX5x series.  It is Vivante instead of AMD, so the new OpenGL ES drivers were developed by Vivante.

View solution in original post

0 Kudos
Reply
1 Reply
853 Views
claymontgomery
Contributor IV

Freescale does not make the source code of their OpenGL ES drivers available.  None of the embedded chip vendors provide that.  Also, the 3D Core in i.MX6 series is different than for the i.MX5x series.  It is Vivante instead of AMD, so the new OpenGL ES drivers were developed by Vivante.

0 Kudos
Reply