porting of OPEN GL drivers for imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

porting of OPEN GL drivers for imx6

ソリューションへジャンプ
1,606件の閲覧回数
Deepu
Contributor III

since I am working on porting of OPENGL drivers for imx6 boards. Can anyone tell me where these driver sources are available.I need to port OPENGL drivers to imx6 which is not using any windowing system (X serve) but with frame buffer support.

タグ(2)
0 件の賞賛
返信
1 解決策
895件の閲覧回数
claymontgomery
Contributor IV

Freescale does not make the source code of their OpenGL ES drivers available.  None of the embedded chip vendors provide that.  Also, the 3D Core in i.MX6 series is different than for the i.MX5x series.  It is Vivante instead of AMD, so the new OpenGL ES drivers were developed by Vivante.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
896件の閲覧回数
claymontgomery
Contributor IV

Freescale does not make the source code of their OpenGL ES drivers available.  None of the embedded chip vendors provide that.  Also, the 3D Core in i.MX6 series is different than for the i.MX5x series.  It is Vivante instead of AMD, so the new OpenGL ES drivers were developed by Vivante.

0 件の賞賛
返信