Hi, all,
I am porting nand driver in u-boot. The nand chip is MT29F2G16ABAE,it conneted with EIM_DA[15..0] of imx53. I have done these works:
1. initial I/O in board-sepcial file-------add setup_nfc() in <uboot>/../mx53_xx.c
2. add nand flash info in type_7[] in annd_device_info.c
add nand driver setup in include/configs/mx53_xx.h,for example, #define CONFIG_SYS_NAND_BASE 0x40000000 etc.
add #define CONFIG_FSL_ENV_ IN_MMC
when the board power up, the error show at the console info is
NAND: No NAND device found!!!
0 MiB
I found that someone say we can add "printf" in drivers under u-boot to debug it. But it ouput nothing to me. And I tried "printk", there is no more infomation to output . I don't know how to debug it.
Can anyone help me?
Regards,
haifeng
Hello!
You should add NAND description in U-Boot and Linux, file drivers/mtd/nand/nand_device_info.c.
Hello,kirill,
I have add nand info in uboot and linux, and I have checked nand_flash_ids[], it seems right.
but the problem still exist.
NAND: No NAND device found!!!
0 MiB
Is there anything what I should do but I leave out ? sorry for my poor english.
Hello!
I see two posssible reason:
- you add NAND description in incorrect table, check this
- you have hardware problem, system can't read identifier from NAND
I think NAND debug can help you locate problem.
P.S. my english also not very good :smileywink:
Hello,kirill,
I'm sure the hardware has no problem because I have tested it in kernel. That is to say I have made it drivers in kernel before, it works well. I can find it and read or write data in it .
Now , I want to boot custom board from nand flash, then I have this problem.
Can you describe the possible reason 1 in details? I have checked the nand_device_info.c , this nand device info should be added in nand_device_info_table_type_7[], it seems there is nothing wrong.
Any more suggestions ?
Regards,
haifeng
I debug it again , it must be problem of initilize fuction. The chip maf_id and device_id should be 0x2c and 0xca,
but the data return are both 0x27 . Let me check it further.
Hello, Hai feng,
Our NAND Flash controller doesn't support 16bit NAND Boot, The basic requirement for NAND device is 2k/4k per page , 8bit data IO.
Regards,
Weidong
Hello, Weidong!
This is not correct, I work with 16-bit NAND Micron MT29F2G16ABBEA, MT29F8G16ABBCA and MT29F8G16ADBDAH4.
Hi,Kirill,
Can you send me a diff file ? My nand chip is MT29F2G16A.
Thank you.
Thank you kirill.
The patch is only nand_device_info.c, I have no problem here.
Can you send me this diff file? directory is <uboot>/drivers/mtd/nand/
mxc_nand.c
Hello!
I not edit it, but you can check NAND configuration in your board configuration file.
I use follow:
/* Support NAND */
#define CONFIG_CMD_NAND
#if defined(CONFIG_CMD_NAND)
#define CONFIG_MXC_NAND
#define CONFIG_SYS_NAND_MAX_CHIPS 8
#define CONFIG_SYS_MAX_NAND_DEVICE 1
#define CONFIG_SYS_NAND_BASE 0x40000000
#define CONFIG_NAND_FW_16BIT 1 /* 1: 16bit 0: 8bit */
#define CONFIG_CMD_FLASH
#define CONFIG_MTD_NAND_VERIFY_WRITE
/* ATTENTION: both NAND have same identificator */
/* use MT29F8G16ABBCA (8Gb, x16, 1.8V) */
/* #define CONFIG_USE_MT29F8G16ABBCA */
/* use MT29F8G16ADBDAH4 (8Gb, x16, 1.8V) */
#define CONFIG_USE_MT29F8G16ADBDAH4
#endif
Hello,kirill,
There are some differences between us.
1. #define CONFIG_SYS_NAND_BASE ,the nand flash address of imx53 should be 0xF7FF0000,I don't know why you use as 0x40000000, although mx53_evk is also 0x40000000.
2. I can't find those definition in imx53 bsp for imx5 cpu.
#define CONFIG_CMD_FLASH
#define CONFIG_MTD_NAND_VERIFY_WRITE
3. The last two definition about MT29F, I think you may use it to distinguish them. I don't understand it's necessary to me because I use the one only.
I have another question. Did you edit nand_hw_eccoob structure in mxc_nand.c? I think the default in bsp does not support MT29F2G16 chip.
The board_nand_init() in mxc_nand.c assign ecc.bytes=9,ecc.layout=&nand_hw_eccoob_512, I think it should be revise according to MT29F2G16.
I think the correct value is ecc.layout=&nand_hw_eccoob_64 , ecc.bytes = 8.
Hello!
1. $ grep CONFIG_SYS_NAND_BASE include/configs/mx53_evk.h
#define CONFIG_SYS_NAND_BASE 0x40000000
What version U-boot you use, I use u-boot-2009.08 from LTIB?
2. $ grep CONFIG_CMD_FLASH include/config_cmd_default.h
#define CONFIG_CMD_FLASH /* flinfo, erase, protect */
No, for drivers/mtd/nand/mxc_nand.c my modification is a very little and not critical, I setup NAND devices in NFC.
Unfortunally now I haven't board with Micron MT29F2G16ABBEA NAND and I can't recheck it work.
Thank you,kirill.
I wish freescale's tech-support group can join our discussion. I am confused about that.
Hello!
Follow my NAND IOMUX comfiguration, hope this help you:
void setup_nand(void)
{
u32 cfg = (PAD_CTL_PKE_ENABLE | PAD_CTL_PUE_PULL |
PAD_CTL_100K_PU | PAD_CTL_ODE_OPENDRAIN_NONE |
PAD_CTL_DRV_HIGH);
clk_config(0, 34, NFC_CLK);
/* EMI NAND_WEIM_DA[0] */
mxc_request_iomux(MX53_PIN_EIM_DA0, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_EIM_DA0, cfg);
/* EMI NAND_WEIM_DA[1] */
mxc_request_iomux(MX53_PIN_EIM_DA1, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_EIM_DA1, cfg);
/* EMI NAND_WEIM_DA[2] */
mxc_request_iomux(MX53_PIN_EIM_DA2, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_EIM_DA2, cfg);
/* EMI NAND_WEIM_DA[3] */
mxc_request_iomux(MX53_PIN_EIM_DA3, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_EIM_DA3, cfg);
/* EMI NAND_WEIM_DA[4] */
mxc_request_iomux(MX53_PIN_EIM_DA4, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_EIM_DA4, cfg);
/* EMI NAND_WEIM_DA[5] */
mxc_request_iomux(MX53_PIN_EIM_DA5, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_EIM_DA5, cfg);
/* EMI NAND_WEIM_DA[6] */
mxc_request_iomux(MX53_PIN_EIM_DA6, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_EIM_DA6, cfg);
/* EMI NAND_WEIM_DA[7] */
mxc_request_iomux(MX53_PIN_EIM_DA7, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_EIM_DA7, cfg);
/* EMI NAND_WEIM_DA[8] */
mxc_request_iomux(MX53_PIN_EIM_DA8, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_EIM_DA8, cfg);
/* EMI NAND_WEIM_DA[9] */
mxc_request_iomux(MX53_PIN_EIM_DA9, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_EIM_DA9, cfg);
/* EMI NAND_WEIM_DA[10] */
mxc_request_iomux(MX53_PIN_EIM_DA10, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_EIM_DA10, cfg);
/* EMI NAND_WEIM_DA[11] */
mxc_request_iomux(MX53_PIN_EIM_DA11, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_EIM_DA11, cfg);
/* EMI NAND_WEIM_DA[12] */
mxc_request_iomux(MX53_PIN_EIM_DA12, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_EIM_DA12, cfg);
/* EMI NAND_WEIM_DA[13] */
mxc_request_iomux(MX53_PIN_EIM_DA13, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_EIM_DA13, cfg);
/* EMI NAND_WEIM_DA[14] */
mxc_request_iomux(MX53_PIN_EIM_DA14, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_EIM_DA14, cfg);
/* EMI NAND_WEIM_DA[15] */
mxc_request_iomux(MX53_PIN_EIM_DA15, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_EIM_DA15, cfg);
/* EMI NANDF_ALE */
mxc_request_iomux(MX53_PIN_NANDF_ALE, IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_NANDF_ALE, cfg | PAD_CTL_HYS_ENABLE);
| /* EMI NANDF_CLE */ | |
| mxc_request_iomux(MX53_PIN_NANDF_CLE, IOMUX_CONFIG_ALT0); | |
| mxc_iomux_set_pad(MX53_PIN_NANDF_CLE, cfg | PAD_CTL_HYS_ENABLE); |
| /* EMI NANDF_CS[0] */ | |
| mxc_request_iomux(MX53_PIN_NANDF_CS0, IOMUX_CONFIG_ALT0); | |
| mxc_iomux_set_pad(MX53_PIN_NANDF_CS0, cfg | PAD_CTL_HYS_ENABLE); |
| /* EMI NANDF_RB[0] */ | |
| mxc_request_iomux(MX53_PIN_NANDF_RB0, IOMUX_CONFIG_ALT0); | |
| mxc_iomux_set_pad(MX53_PIN_NANDF_RB0, cfg | PAD_CTL_HYS_ENABLE); |
| /* EMI NANDF_RB_B */ | |
| mxc_request_iomux(MX53_PIN_NANDF_RE_B, IOMUX_CONFIG_ALT0); | |
| mxc_iomux_set_pad(MX53_PIN_NANDF_RE_B, cfg | PAD_CTL_HYS_ENABLE); |
| /* EMI NANDF_WE_B */ | |
| mxc_request_iomux(MX53_PIN_NANDF_WE_B, IOMUX_CONFIG_ALT0); | |
| mxc_iomux_set_pad(MX53_PIN_NANDF_WE_B, cfg | PAD_CTL_HYS_ENABLE); |
| /* EMI NANDF_WP_B */ | |
| mxc_request_iomux(MX53_PIN_NANDF_WP_B, IOMUX_CONFIG_ALT0); | |
| mxc_iomux_set_pad(MX53_PIN_NANDF_WP_B, cfg | PAD_CTL_HYS_ENABLE); |
}
Hi Haifeng,
Sorry for my mistake ! I confused i.mx6 and i.mx53. yes, you are right, i.MX53 supports 16bit NAND Flash.
Regards,
Weidong
Hi,weidong,
As what I have described above,what I should do or how to port nand driver in uboot?
I don't know what's wrong that I have done.
Hi,weidong,
Thank you for your quick reply. I check the reference manual again, find that it can be set to 4bit ECC when page size is 512B/2K/4K(chapter 7.5.2 , Table 7-11). Can you tell me what's your meaning?