pmic powerup problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pmic powerup problem

2,728件の閲覧回数
saida
Contributor II

hi i.mx6 community

in my custom made board based on i.mx6 the pmic is not startsup

i am using pmic MMF0100NP device and when  power is given switch3 voltage 1.5v is coming remaining or not but standby signal is high

to make it low i shorted to ground through a jumper even voltages are not coming what could be the problem ?

please can any one help me in this regsrd

thanks and regards

saida

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,380件の閲覧回数
angelo_d
Senior Contributor I

Hi

are you talking about 1V5 for DDR in pin 38?

reasons for that PS to miss are many:

- compare carefully the schematic with a similar board, as sabreauto maybe, well-known to work

- something wrong in the connected DDR, so once disconnected from the PMIC you should se the correct 1.5

also, never short pins directly to GND or VCC, always use a resistor.

0 件の賞賛
返信

2,380件の閲覧回数
saida
Contributor II

hi

no i am getting DDR voltage from PMIC switch3 but problem is that reaminig i am not getting

one more thing is PMIC is getting hot

thanks and regards

saida

0 件の賞賛
返信

2,380件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI saida

if chip is overheating it may turn off its supplies, recommended to

check connections using AN4717 AN4717, Schematic Guidelines for the MMPF0100

Also MMF0100NP (not programmed) should not be used with i.MX6,

please use programmed parts, given in Table 1. Orderable Part Variations MMPF0100

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,380件の閲覧回数
saida
Contributor II

Hi

ok i will change to F0 part than i will come back to you and i went throgh AN4717 before design its fine

thank you

0 件の賞賛
返信