platform_driver struct proper usage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

platform_driver struct proper usage

1,837件の閲覧回数
john_smith
Contributor II

Hello!

I have noticed that GPU driver's suspend/resume callbacks are never called. These callbacks are registered in such a way (drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_probe.c):

static struct platform_driver gpu_driver = {
    .probe      = gpu_probe,
#if LINUX_VERSION_CODE >= KERNEL_VERSION(3, 8, 0)
    .remove     = gpu_remove,
#else
    .remove     = __devexit_p(gpu_remove),
#endif

    .suspend    = gpu_suspend,
    .resume     = gpu_resume,

    .driver     = {
        .owner = THIS_MODULE,
        .name   = DEVICE_NAME,
#if defined(CONFIG_PM) && LINUX_VERSION_CODE >= KERNEL_VERSION(2, 6, 30)
        .pm     = &gpu_pm_ops,
#endif
    }
};

In init() function:

platform_driver_register(&gpu_driver);

But when we try echo freeze > sys/power/state (or any other power-down mode) we see that functions gpu_suspend() and gpu_resume() are never being called.

What can be the reason of it?

P.S. - SabreSD board, official Android 6 from nxp, linux kernel v4.1.15.

ラベル(3)
0 件の賞賛
返信
1 返信

1,641件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi John

reason may be that in low power modes gpu power is turned of

(which seems as better method), one can check VDD_PU_CAP

in Figure 50-1. Power system overview i.MX6DQ RM.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信